Z-Stack API Reference  6.30.00.23
gpPairingCmd_t Struct Reference

Data Fields

uint32_t options
 Options field of the GP Pairing command.
 
uint32_t gpdId
 ID of the GPD.
 
uint8_t gpdIEEE [Z_EXTADDR_LEN]
 0b010. More...
 
uint8_t ep
 is 0b010. More...
 
uint8_t sinkIEEE [Z_EXTADDR_LEN]
 Sink IEEE address value.
 
uint16_t sinkNwkAddr
 Sink Network address value.
 
uint16_t sinkGroupID
 Sink group ID value.
 
uint8_t deviceId
 The DeviceID for GPD.
 
uint32_t gpdSecCounter
 The security frame counter.
 
uint8_t gpdKey [SEC_KEY_LEN]
 The security key for the GPD.
 
uint16_t assignedAlias
 The commissioned alias for this GPD.
 
uint8_t forwardingRadius
 To limit the range of the groupcast.
 

Field Documentation

§ ep

uint8_t ep

is 0b010.

Endpoint of the GP if application ID

§ gpdIEEE

uint8_t gpdIEEE[Z_EXTADDR_LEN]

0b010.

IEEE of the GPD if application ID is


The documentation for this struct was generated from the following file: