![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.07.00
|
Structure of NV data for the connected device's address information. More...
Data Fields | |
uint8_t | addr [B_ADDR_LEN] |
GAP_Peer_Addr_Types_t | addrType |
uint8_t | stateFlags |
Structure of NV data for the connected device's address information.
uint8_t addr[B_ADDR_LEN] |
Peer's address
If identity information exists for this bond, this will be an identity address
GAP_Peer_Addr_Types_t addrType |
Peer's address type
uint8_t stateFlags |
State flags of bond
GAP_BONDED_STATE_FLAGS