TI BLE5-Stack API Documentation  2.02.07.00
Data Structures | Macros | Enumerations | Functions
gap_advertiser.h File Reference

Detailed Description

GAP Advertiser layer interface.

Go to the source code of this file.

Data Structures

struct  GapAdv_params_t
 
struct  GapAdv_periodicAdvData_t
 Periodic advertising data structure. More...
 
struct  GapAdv_periodicAdvParams_t
 Periodic advertising parameters structure. More...
 
struct  GapAdv_scanReqReceived_t
 Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event. More...
 
struct  GapAdv_setTerm_t
 Data type returned with GAP_EVT_ADV_SET_TERMINATED event. More...
 
struct  GapAdv_truncData_t
 Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event. More...
 

Macros

#define GAP_ADV_INVALID_HANDLE   0xFF
 Invalid Advertising Handle for GAP Advertising API's.
 
#define GAP_ADV_TX_POWER_NO_PREFERENCE   127
 Allow the controller to choose the Tx power.
 
#define GAPADV_PARAMS_AE_LONG_RANGE_CONN
 Default parameters for long range, connectable, advertising extension. More...
 
#define GAPADV_PARAMS_AE_NC_NS
 Non-Connectable & Non-Scannable advertising set. More...
 
#define GAPADV_PARAMS_LEGACY_SCANN_CONN
 Default parameters for legacy, scannable, connectable advertising. More...
 
#define GAPADV_PERIODIC_ADV_DATA_COMPLETE   0x03
 Periodic Advertising operation options - Complete data.
 
#define GAPADV_PERIODIC_ADV_DATA_FIRST_FRAG   0x01
 Periodic Advertising operation options - First fragment.
 
#define GAPADV_PERIODIC_ADV_DATA_INTERMIDIATE_FRAG   0x00
 Periodic Advertising operation options - Intermidiate fragment.
 
#define GAPADV_PERIODIC_ADV_DATA_LAST_FRAG   0x02
 Periodic Advertising operation options - Last fragment.
 
#define GAPADV_PERIODIC_ADV_DISABLE_TX_POWER   0x0000
 Periodic Advertising - Disable TX power property.
 
#define GAPADV_PERIODIC_ADV_ENABLE_TX_POWER   0x0040
 Periodic Advertising - Enable TX power property.
 
#define GAPADV_PERIODIC_ADV_INTERVAL_MAX   0xFFFF
 Periodic Advertising - Maximum interval.
 
#define GAPADV_PERIODIC_ADV_INTERVAL_MIN   0x0006
 Periodic Advertising - Minimum interval.
 
#define GAPADV_PERIODIC_ADV_MAX_DATA_LEN   252
 Periodic Advertising - Maximum fragment/complete data length.
 

Enumerations

enum  GapAdv_advChannels_t {
  GAP_ADV_CHAN_37 = BV(0), GAP_ADV_CHAN_38 = BV(1), GAP_ADV_CHAN_39 = BV(2), GAP_ADV_CHAN_37_38,
  GAP_ADV_CHAN_37_39, GAP_ADV_CHAN_38_39, GAP_ADV_CHAN_ALL
}
 GAP Advertiser Defines for Advertiser Channels. More...
 
enum  GapAdv_dataTypes_t { GAP_ADV_DATA_TYPE_ADV, GAP_ADV_DATA_TYPE_SCAN_RSP }
 Gap Advertising Data Types. More...
 
enum  GapAdv_enableOptions_t { GAP_ADV_ENABLE_OPTIONS_USE_MAX, GAP_ADV_ENABLE_OPTIONS_USE_DURATION, GAP_ADV_ENABLE_OPTIONS_USE_MAX_EVENTS }
 Enable options for GapAdv_enable. More...
 
enum  GapAdv_eventMaskFlags_t {
  GAP_ADV_EVT_MASK_SCAN_REQ_NOTI = AE_NOTIFY_ENABLE_SCAN_REQUEST, GAP_ADV_EVT_MASK_SET_TERMINATED = BV(1), GAP_ADV_EVT_MASK_START_AFTER_ENABLE = AE_NOTIFY_ENABLE_ADV_SET_START, GAP_ADV_EVT_MASK_START = AE_NOTIFY_ENABLE_ADV_START,
  GAP_ADV_EVT_MASK_END = AE_NOTIFY_ENABLE_ADV_END, GAP_ADV_EVT_MASK_END_AFTER_DISABLE = AE_NOTIFY_ENABLE_ADV_SET_END, GAP_ADV_EVT_MASK_ALL
}
 
enum  GapAdv_eventProps_t {
  GAP_ADV_PROP_CONNECTABLE = BV(0), GAP_ADV_PROP_SCANNABLE = BV(1), GAP_ADV_PROP_DIRECTED = BV(2), GAP_ADV_PROP_HDC = BV(3),
  GAP_ADV_PROP_LEGACY = BV(4), GAP_ADV_PROP_ANONYMOUS = BV(5), GAP_ADV_PROP_TX_POWER = BV(6)
}
 GAP Advertising Event Param Properties. More...
 
enum  GapAdv_filterPolicy_t { GAP_ADV_WL_POLICY_ANY_REQ, GAP_ADV_WL_POLICY_WL_SCAN_REQ, GAP_ADV_WL_POLICY_WL_CONNECT_IND, GAP_ADV_WL_POLICY_WL_ALL_REQ }
 GAP Advertiser White List Policy. More...
 
enum  GapAdv_freeBufferOptions_t { GAP_ADV_FREE_OPTION_DONT_FREE, GAP_ADV_FREE_OPTION_ADV_DATA, GAP_ADV_FREE_OPTION_SCAN_RESP_DATA }
 Possible free options for Gap Advertiser API's. More...
 
enum  GapAdv_ParamId_t {
  GAP_ADV_PARAM_PROPS, GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX, GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP,
  GAP_ADV_PARAM_PEER_ADDRESS_TYPE, GAP_ADV_PARAM_PEER_ADDRESS, GAP_ADV_PARAM_FILTER_POLICY, GAP_ADV_PARAM_TX_POWER,
  GAP_ADV_PARAM_PRIMARY_PHY, GAP_ADV_PARAM_SECONDARY_PHY, GAP_ADV_PARAM_SID
}
 
enum  GapAdv_primaryPHY_t { GAP_ADV_PRIM_PHY_1_MBPS = 0x01, GAP_ADV_PRIM_PHY_CODED_S8 = 0x03, GAP_ADV_PRIM_PHY_CODED_S2 = 0x83 }
 Gap Advertiser Options for advertising on the primary PHY. More...
 
enum  GapAdv_secondaryPHY_t { GAP_ADV_SEC_PHY_1_MBPS = 0x01, GAP_ADV_SEC_PHY_2_MBPS = 0x02, GAP_ADV_SEC_PHY_CODED_S8 = 0x03, GAP_ADV_SEC_PHY_CODED_S2 = 0x83 }
 Gap Advertiser Options for advertising on the secondary PHY. More...
 

Functions

bStatus_t GapAdv_abortLoad (void)
 
bStatus_t GapAdv_create (pfnGapCB_t *cb, GapAdv_params_t *advParam, uint8 *advHandle)
 
bStatus_t GapAdv_destroy (uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
 
bStatus_t GapAdv_disable (uint8 handle)
 Disable an active advertising set. More...
 
bStatus_t GapAdv_enable (uint8 handle, GapAdv_enableOptions_t enableOptions, uint16 durationOrMaxEvents)
 
bStatus_t GapAdv_getBuffer (uint8 handle, GapAdv_dataTypes_t dataType, uint16 *pLen, uint8 **ppBuf)
 
bStatus_t GapAdv_getParam (uint8 handle, GapAdv_ParamId_t paramID, void *pValue, uint8_t *pLen)
 
bStatus_t GapAdv_loadByBuffer (uint16 len, uint8 *pBuf)
 
bStatus_t GapAdv_loadByBuffer_hook (uint16 len, uint8 *pBuf)
 
bStatus_t GapAdv_loadByHandle (uint8 handle, GapAdv_dataTypes_t dataType, uint16 len, uint8 *pBuf)
 
bStatus_t GapAdv_prepareLoadByBuffer (uint8 *pBuf, bool freeOldData)
 
bStatus_t GapAdv_prepareLoadByHandle (uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
 
bStatus_t GapAdv_setEventMask (uint8 handle, GapAdv_eventMaskFlags_t mask)
 
bStatus_t GapAdv_setParam (uint8 handle, GapAdv_ParamId_t paramID, void *pValue)
 
bStatus_t GapAdv_SetPeriodicAdvData (uint8 advHandle, GapAdv_periodicAdvData_t *periodicAdvData)
 
bStatus_t GapAdv_SetPeriodicAdvEnable (uint8 enable, uint8 advHandle)
 
uint8_t GapAdv_SetPeriodicAdvParams (uint8 advHandle, GapAdv_periodicAdvParams_t *periodicAdvParams)
 
bStatus_t GapAdv_setVirtualAdvAddr (uint8 advHandle, uint8 *bdAddr)
 
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale