TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
GapAdv_periodicAdvParams_t Struct Reference

Periodic advertising parameters structure. More...

Data Fields

uint16 periodicAdvIntervalMax
 Maximum periodic advertising interval; Range: 0x0006 to 0xFFFF Time = N * 1.25 ms Time Range: 7.5ms to 81.91875s.
 
uint16 periodicAdvIntervalMin
 Minimum periodic advertising interval; Range: 0x0006 to 0xFFFF Time = N * 1.25 ms Time Range: 7.5ms to 81.91875s.
 
uint16 periodicAdvProp
 Periodic advertising properties - set bit 6 for include TxPower in the advertising PDU.
 

Detailed Description

Periodic advertising parameters structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale