DMM API Reference  4.30.00.19
dmm_scheduler.h File Reference

Detailed Description

Dual Mode Manager Scheduler.


DMM enables devices to run multiple wireless protocol stacks concurrently. The DMMSch is to enable concurrent operation of multiple stacks with minimized conflicts so that it does not cause significant performance degradation. The DMMSch uses Application Level, Stack Level information, and Global Priority Table (GPT) when scheduling a command. Stack Level information (provided by stack) is embedded in each RF command and it includes:

  • Start Type, Start Time, AllowDelay, Priority, Activity, etc. Application Level information (provided by User via the Policy Table) includes:
  • Application State Name, Weight, AppliedActivity, Pause, etc. Global Priority Table (GPT)
  • GPT defines relative priorities of the two stacks The DMMSch uses Start Type, Start Time, and AllowDelay (Stack Level Information) when scheduling a RF command and tries to avoid a conflict by delaying the command if allowed. When a command conflicts with another (during scheduling or execution), The DMMSch selects one command over the other based on the final priority of two commands as below: Final Priority = GPT (Stack level priority) + weight (Application Level)

DMMSch API

To use the DMMSch module to schedule a tacks RF commands, the application calls the following APIs:

  • DMMSch_init(): Initialize the DMMSch module/task.
  • DMMSch_Params_init(): Initialize a DMMSch_Params structure with default values. Then change the parameters from non-default values as needed.
  • DMMSch_open(): Open an instance of the DMMSch module, passing the initialized parameters.
  • Stack A application - DMMSch_registerClient: Passes Task_Handle and StackRole so DMMSch can map the Task_Handle to the stack role
  • Stack A application - Rf_open -> DMMSch_rfOpen: DMMSch overwrites the RF_Mode and rf patches for multi-mode operation, maps RF Handle to the stack ID, assigns phySwitchingTime for DMM operation. From this point, Task_Handle, StackRole, and Stack ID are all related.
  • Stack B application - DMMSch_registerClient: Passes Task_Handle and StackRole so DMMSch can map the Task_Handle to the stack role
  • Stack B application - Rf_open -> DMMSch_rfOpen: Rf_open -> DMMSch_rfOpen: DMMSch overwrites the RF_Mode and rf patches for multi-mode operation, maps RF Handle to the stack ID, assigns phySwitchingTime for DMM operation. From this point, Task_Handle, StackRole, and Stack ID are all related.
  • Stack A application - RF_scheduleCmd -> DMMSch_rfScheduleCmd: DMMSch adjusted timing based on policy
  • Stack B application - RF_scheduleCmd -> DMMSch_rfScheduleCmd: DMMSch adjusted timing based on policy
#include "stdint.h"
#include <ti/drivers/rf/RF.h>
#include <ti/sysbios/knl/Task.h>
#include "dmm_policy.h"

Go to the source code of this file.

Classes

struct  DMMSch_Params
 RF parameter struct DMM Scheduler parameters are used with the DMMSch_open() and DMMSch_Params_init() call. More...
 

Macros

#define CONFLICT_FLUSH_ALL   1
 Define to flush all commands. More...
 
#define xDMM_DEBUG_LOGGING
 DMM Debug Logging. More...
 
#define DMM_dbgLog0(str)
 
#define DMM_dbgLog1(str, a0)
 
#define DMM_dbgLog2(str, a0, a1)
 
#define DMM_dbgLog3(str, a0, a1, a2)
 
#define DMM_dbgLog4(str, a0, a1, a2, a3)
 
#define DMM_dbgLog5(str, a0, a1, a2, a3, a4)
 

Typedefs

typedef void(* DMMSch_PreemptionCb) (DMMPolicy_StackRole stackRolePreempted)
 Defines the preemption callback. More...
 

Enumerations

enum  DMM_ConflictStatus { DMM_NoConflict = 0, DMM_ConflictWithPrev, DMM_ConflictWithNext, DMM_ConfictWithBoth }
 DMM Conflict struct DMM Conflict Status. More...
 

Functions

void DMMSch_Params_init (DMMSch_Params *params)
 Function to initialize the DMMSch_Params struct to its defaults. More...
 
void DMMSch_init (void)
 Function that initializes the DMMSch module. More...
 
void DMMSch_registerPreemptionCb (DMMSch_PreemptionCb dmmSchPreemptionCb)
 allows policy manager to register a callback on command preemption More...
 
void DMMSch_open (DMMSch_Params *params)
 Function to open the DMMSch module. More...
 
void DMMSch_registerClient (Task_Handle *pTaskHndl, DMMPolicy_StackRole StackRole)
 Register an DMM Scheduler client. More...
 
RF_Handle DMMSch_rfOpen (RF_Object *pObj, RF_Mode *pRfMode, RF_RadioSetup *pOpSetup, RF_Params *params)
 Intercepts calls from a stack to RF_postCmd (re-mapped to DMMSch_rfOpen), The DMMSch module uses this to tie. More...
 
RF_CmdHandle DMMSch_rfPostCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
 Handles calls from a stack to RF_postCmd (re-mapped to DMMSch_postCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd. More...
 
RF_CmdHandle DMMSch_rfScheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
 Handles calls from a stack to RF_scheduleCmd (re-mapped to DMMSch_scheduleCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd. More...
 
RF_EventMask DMMSch_rfRunCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
 Handles calls from a stack to RF_runCmd (re-mapped to DMMSch_runCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd. More...
 
RF_EventMask DMMSch_rfRunScheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
 Handles calls from a stack to RF_runScheduleCmd (re-mapped to DMMSch_runScheduleCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd. More...
 
RF_Stat DMMSch_rfCancelCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode)
 Abort/stop/cancel single command in command queue. More...
 
RF_Stat DMMSch_rfFlushCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode)
 Abort/stop/cancel command and any subsequent commands in command queue. More...
 
RF_Stat DMMSch_rfRunImmediateCmd (RF_Handle h, uint32_t *pCmdStruct)
 Send any Immediate command.
More...
 
RF_Stat DMMSch_rfRunDirectCmd (RF_Handle h, uint32_t cmd)
 Send any Direct command.
More...
 
bool DMMSch_setBlockModeOn (DMMPolicy_StackRole stackRole)
 Turn on Block mode. More...
 
bool DMMSch_setBlockModeOff (DMMPolicy_StackRole stackRole)
 Turn off Block mode. More...
 
bool DMMSch_getBlockModeStatus (DMMPolicy_StackRole stackRole)
 Get Block mode status. More...
 
RF_Stat DMMSch_rfRequestAccess (RF_Handle h, RF_AccessParams *pParams)
 Request access RF API that should not be used in DMM

 

Macro Definition Documentation

§ CONFLICT_FLUSH_ALL

#define CONFLICT_FLUSH_ALL   1

Define to flush all commands.

Default option to flush all commands for a specific client for a conflict

§ xDMM_DEBUG_LOGGING

#define xDMM_DEBUG_LOGGING

DMM Debug Logging.

Debugging for internal use only.

Typedef Documentation

§ DMMSch_PreemptionCb

typedef void(* DMMSch_PreemptionCb) (DMMPolicy_StackRole stackRolePreempted)

Defines the preemption callback.

The function is invoked when a preemption occurs in DMM Scheduler.

The arguments are:

  • stackRolePreempted stack role for command was preempted.

Enumeration Type Documentation

§ DMM_ConflictStatus

DMM Conflict struct DMM Conflict Status.

Enumerator
DMM_NoConflict 

used to define where there is no conflict in commands.

DMM_ConflictWithPrev 

used to define where there is a conflict with the previous command.

DMM_ConflictWithNext 

used to define where there is a conflict with the next command.

DMM_ConfictWithBoth 

used to define where there is a conflict with both previous and next command.

Function Documentation

§ DMMSch_getBlockModeStatus()

bool DMMSch_getBlockModeStatus ( DMMPolicy_StackRole  stackRole)

Get Block mode status.

Parameters
stackRolestack role associated with Task handle
Returns
true: Block Mode is On, False: Block Mode is Off

§ DMMSch_init()

void DMMSch_init ( void  )

Function that initializes the DMMSch module.

§ DMMSch_open()

void DMMSch_open ( DMMSch_Params params)

Function to open the DMMSch module.

Parameters
paramsAn pointer to RF_Params structure for initialization

§ DMMSch_Params_init()

void DMMSch_Params_init ( DMMSch_Params params)

Function to initialize the DMMSch_Params struct to its defaults.

Parameters
paramsAn pointer to RF_Params structure for initialization

Defaults values are:

§ DMMSch_registerClient()

void DMMSch_registerClient ( Task_Handle *  pTaskHndl,
DMMPolicy_StackRole  StackRole 
)

Register an DMM Scheduler client.

Parameters
pTaskHndlRTOS Thread handle that the stack is running in, used to map the RF Client handle to a stack role
StackRolestack role associated with Task handle

§ DMMSch_registerPreemptionCb()

void DMMSch_registerPreemptionCb ( DMMSch_PreemptionCb  dmmSchPreemptionCb)

allows policy manager to register a callback on command preemption

Parameters
dmmSchPreemptionCbcallback to register

§ DMMSch_rfCancelCmd()

RF_Stat DMMSch_rfCancelCmd ( RF_Handle  h,
RF_CmdHandle  ch,
uint8_t  mode 
)

Abort/stop/cancel single command in command queue.

If command is running, aborts/stops it and posts callback for the aborted/stopped command.
If command has not yet run, cancels it it and posts callback for the cancelled command.
If command has already run or been aborted/stopped/cancelled, has no effect.
If RF_cancelCmd is called from a Swi context with same or higher priority than RF Driver Swi, when the RF core is powered OFF -> the cancel callback will be delayed until the next power-up cycle.

Note
Calling context : Task/SWI
Parameters
hHandle previously returned by RF_open()
chCommand handle previously returned by RF_postCmd().
mode1: Stop gracefully, 0: abort abruptly
Returns
RF_Stat indicates if command was successfully completed

§ DMMSch_rfFlushCmd()

RF_Stat DMMSch_rfFlushCmd ( RF_Handle  h,
RF_CmdHandle  ch,
uint8_t  mode 
)

Abort/stop/cancel command and any subsequent commands in command queue.

If command is running, aborts/stops it and then cancels all later commands in queue.
If command has not yet run, cancels it and all later commands in queue.
If command has already run or been aborted/stopped/cancelled, has no effect.
The callbacks for all cancelled commands are issued in chronological order.
If RF_flushCmd is called from a Swi context with same or higher priority than RF Driver Swi, when the RF core is powered OFF -> the cancel callback will be delayed until the next power-up cycle.

Note
Calling context : Task/SWI
Parameters
hHandle previously returned by RF_open()
chCommand handle previously returned by RF_postCmd().
mode1: Stop gracefully, 0: abort abruptly
Returns
RF_Stat indicates if command was successfully completed

§ DMMSch_rfOpen()

RF_Handle DMMSch_rfOpen ( RF_Object *  pObj,
RF_Mode *  pRfMode,
RF_RadioSetup *  pOpSetup,
RF_Params *  params 
)

Intercepts calls from a stack to RF_postCmd (re-mapped to DMMSch_rfOpen), The DMMSch module uses this to tie.

Parameters
pObjpointer to RF Object
pRfModepointer to RF Mode
pOpSetuppointer to Radio Setup
paramspointer to RF params
Returns
An pointer to RF_Params structure for initialization

§ DMMSch_rfPostCmd()

RF_CmdHandle DMMSch_rfPostCmd ( RF_Handle  h,
RF_Op *  pOp,
RF_Priority  ePri,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Handles calls from a stack to RF_postCmd (re-mapped to DMMSch_postCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd.

See also
RF_pendCmd(), RF_runCmd(), RF_scheduleCmd(), RF_RF_cancelCmd(), RF_flushCmd(), RF_getCmdOp()
Parameters
hDriver handle previously returned by RF_open()
pOpPointer to the RF operation command.
ePriPriority of this RF command (used for arbitration in multi-client systems)
pCbCallback function called during command execution and upon completion. If RF_postCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback or that can be pended on.
Returns
A handle to the RF command. Return value of RF_ALLOC_ERROR indicates error.

§ DMMSch_rfRunCmd()

RF_EventMask DMMSch_rfRunCmd ( RF_Handle  h,
RF_Op *  pOp,
RF_Priority  ePri,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Handles calls from a stack to RF_runCmd (re-mapped to DMMSch_runCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd.

Parameters
hDriver handle previously returned by RF_open()
pOpPointer to the RF operation command.
ePriPriority of this RF command (used for arbitration in multi-client systems)
pCbCallback function called during command execution and upon completion. If RF_runCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback or that can be pended on.
Returns
The relevant termination event.

§ DMMSch_rfRunDirectCmd()

RF_Stat DMMSch_rfRunDirectCmd ( RF_Handle  h,
uint32_t  cmd 
)

Send any Direct command.

Direct Comamnd value is send to RDBELL immediately, if radio is active and the RF_Handle point to the current client.
In other appropriate RF_Stat values are returned.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
cmdDirect command value.
Returns
RF_Stat indicates if command was successfully completed.

§ DMMSch_rfRunImmediateCmd()

RF_Stat DMMSch_rfRunImmediateCmd ( RF_Handle  h,
uint32_t *  pCmdStruct 
)

Send any Immediate command.

Immediate Comamnd is send to RDBELL, if radio is active and the RF_Handle points to the current client.
In other appropriate RF_Stat values are returned.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
pCmdStructPointer to the immediate command structure
Returns
RF_Stat indicates if command was successfully completed

§ DMMSch_rfRunScheduleCmd()

RF_EventMask DMMSch_rfRunScheduleCmd ( RF_Handle  h,
RF_Op *  pOp,
RF_ScheduleCmdParams *  pSchParams,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Handles calls from a stack to RF_runScheduleCmd (re-mapped to DMMSch_runScheduleCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd.

Parameters
hHandle previously returned by RF_open()
pOpPointer to the RF_Op. Must normally be in persistent and writeable memory
pSchParamsPointer to the schdule command parameter structure
pCbCallback function called upon command completion (and some other events). If RF_runScheduleCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback.
Returns
The relevant command completed event.

§ DMMSch_rfScheduleCmd()

RF_CmdHandle DMMSch_rfScheduleCmd ( RF_Handle  h,
RF_Op *  pOp,
RF_ScheduleCmdParams *  pSchParams,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Handles calls from a stack to RF_scheduleCmd (re-mapped to DMMSch_scheduleCmd), adjusts timing as necessary and schedules then accordingly with RF_scheduleCmd.

Parameters
hHandle previously returned by RF_open()
pOpPointer to the RF_Op. Must normally be in persistent and writeable memory
pSchParamsPointer to the schedule command parameter structure
pCbCallback function called upon command completion (and some other events). If RF_scheduleCmd() fails no callback is made
bmEventBitmask of events that will trigger the callback.
Returns
A handle to the RF command. Return value of RF_ALLOC_ERROR indicates error.

§ DMMSch_setBlockModeOff()

bool DMMSch_setBlockModeOff ( DMMPolicy_StackRole  stackRole)

Turn off Block mode.

Parameters
stackRolestack role associated with Task handle
Returns
true: success, false: the stack role cannot be found

§ DMMSch_setBlockModeOn()

bool DMMSch_setBlockModeOn ( DMMPolicy_StackRole  stackRole)

Turn on Block mode.

Parameters
stackRolestack role associated with Task handle
Returns
true: success, false: the stack role cannot be found