Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
AESCTRDRBG.h File Reference

Detailed Description

AESCTRDRBG driver header.


Overview

AESCTRDRBG is a cryptographically secure deterministic random bit generator that is used to efficiently generate random numbers for use in keying material or other security related purposes. It is based on the AES block cipher operating in Counter (CTR) mode and is defined by NIST SP 800-90A.

AESCTRDRBG derives a sequence of pseudo-random numbers based on an initial secret seed and additional, non-secret personalization data provided during instantiation. A sequence of random bits generated by AESCTRDRBG will have an equivalent entropy content of MIN(sequenceLength, security strength). The security strength is based on the seed length and the AES key length used in the AESCTRDRBG instance.

AES-128 AES-192 AES-256
Security Strength (bits) 128 192 256
Seed Length (bits) 192 320 384
Personalization String Length (bits) <= 192 <= 320 <= 384
Max Requests Between Reseeds 2^48 2^48 2^48
Max Request Length (bits) 2^19 2^19 2^19

Security Strength

The seed must be sourced from a cryptographically secure source such as a True Random Number Generator and contain seed length bits of entropy. Since the seed length is always larger than the security strength for any one AES key length, the output of one AESCTRDRBG instance may not be used to seed another instance of the same or higher security strength.

Reseeding

Because of the way AES CTR operates, there are a limited number of output bitstreams that may be generated before the AESCTRDRBG instance must be reseeded. The reseeding interval is set by the number of random bit sequences generated and not by their individual or combined lengths. Each time random bits are requested of the AESCTRDRBG instance by the application, the reseed counter is incremented by one regardless of how many bits at a time are requested. When this counter reaches the configured reseed limit, the AESCTRDRBG instance will return AESCTRDRBG_STATUS_RESEED_REQUIRED until it is reseeded.

The maximum permitted number of requests between reseeds is 2^48. The default counter is only 2^32 long for ease of implementation. A more conservative reseed limit may be configured by the application for increased security.

A previously used seed may never be reused to reseed an AESCTRDRBG instance. The seed used to instantiate or reseed an instance must be generated by an approved entropy source.

Derivation Function

NIST specifies the the use of an optional derivation function to reduced entropy and personalization string lengths longer than the seed length down to the seed length. This feature is not presently supported.

Usage

This documentation provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the APIs are provided in subsequent sections.

Synopsis

// Instantiate the AESCTRDRBG instance
params.keyLength = AESCTRDRBG_AES_KEY_LENGTH_128;
params.reseedInterval = 0xFFFFFFFF;
params.seed = seedBuffer;
handle = AESCTRDRBG_open(0, &params);
result = AESCTRDRBG_generateKey(handle, &resultKey);
reseedResult = AESCTRDRBG_reseed(handle, reseedBuffer, NULL, 0);

Examples

Instantiating an AESCTRDRBG Instance with TRNG

...
TRNG_Handle trngHandle;
int_fast16_t result;
uint8_t seedBuffer[AESCTRDRBG_SEED_LENGTH_AES_128];
// Open a TRNG driver instance
trngHandle = TRNG_open(0, NULL);
if (trngHandle == NULL) {
// Failed to open TRNG instance
while(1);
}
// Generate entropy for the seed
result = TRNG_getRandomBytes(trngHandle, seedBuffer, AESCTRDRBG_SEED_LENGTH_AES_128);
if (result != TRNG_STATUS_SUCCESS) {
// Failed to generate entropy
while(1);
}
TRNG_close(trngHandle);
// Instantiate the AESCTRDRBG parameters and the driver instance
params.reseedInterval = 0xFFFFFFFF;
params.seed = seedBuffer;
handle = AESCTRDRBG_open(0, &params);
if (handle == NULL) {
// Failed to open AESCTRDRBG instance
while(1);
}

Generating random key with Reseeding

...
#define RANDOM_KEY_LENGTH_BYTES 32
TRNG_Handle trngHandle;
CryptoKey randomKey;
int_fast16_t result;
uint8_t randomKeyBuffer[RANDOM_KEY_LENGTH_BYTES];
// Initialise the AESCTRDRBG params and driver instance here
...
// Initialize a blank CryptoKey
CryptoKeyPlaintext_initBlankKey(&randomKey, randomKeyBuffer, RANDOM_KEY_LENGTH_BYTES);
// Generate key-material for the CryptoKey
result = AESCTRDRBG_generateKey(handle, &randomKey);
// Check return value and reseed if needed. This should happen only after many invocations
// of AESCTRDRBG_generateKey().
TRNG_Handle trngHandle;
int_fast16_t reseedResult;
uint8_t reseedBuffer[AESCTRDRBG_SEED_LENGTH_AES_128];
reseedResult = TRNG_getRandomBytes(trngHandle, reseedBuffer, AESCTRDRBG_SEED_LENGTH_AES_128);
if (reseedResult != TRNG_STATUS_SUCCESS) {
// Failed to generate entropy
while(1);
}
TRNG_close(trngHandle);
// Reseed the DRBG instance
reseedResult = AESCTRDRBG_reseed(handle, reseedBuffer, NULL, 0);
if (reseedResult != AESCTRDRBG_STATUS_SUCCESS) {
// Failed to reseed the DRBG instance
while(1);
}
// If AESCTRDRBG_STATUS_RESEED_REQUIRED was returned from the previous call to
// AESCTRDRBG_generateKey(), the random key was never generated by that call.
// So the user must invoke that call again (after reseeding) to get a random key.
result = AESCTRDRBG_generateKey(handle, &randomKey);
if (result != AESCTRDRBG_STATUS_SUCCESS) {
// Failed to generate key-material
while(1);
}
}
else if (result != AESCTRDRBG_STATUS_SUCCESS) {
// Failed to generate key-material
while(1);
}

Generating random bytes output to an array

...
#define RANDOM_BYTES_SIZE 16
TRNG_Handle trngHandle;
int_fast16_t result;
uint8_t randomBytesBuffer[RANDOM_BYTES_SIZE];
// Initialise the AESCTRDRBG params and driver instance here
...
// Get random bytes output to the buffer/array
result = AESCTRDRBG_getRandomBytes(handle, &randomBytesBuffer, RANDOM_BYTES_SIZE);
// Check and reseed if required. This should happen only after many invocations
// of AESCTRDRBG_getRandomBytes().
// Reseed the DRBG instance using AESCTRDRBG_reseed()
// and invoke AESCTRDRBG_getRandomBytes() similar to the previous example.
}
else if (result != AESCTRDRBG_STATUS_SUCCESS) {
// Failed to generate random bytes
while(1);
}
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESCTR.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for AESCTRDRBG.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESCTRDRBG_Params
 AESCTRDRBG Parameters. More...
 

Macros

#define AESCTRDRBG_STATUS_RESERVED   AES_STATUS_RESERVED
 
#define AESCTRDRBG_STATUS_SUCCESS   AES_STATUS_SUCCESS
 Successful status code. More...
 
#define AESCTRDRBG_STATUS_ERROR   AES_STATUS_ERROR
 Generic error status code. More...
 
#define AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define AESCTRDRBG_STATUS_RESEED_REQUIRED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 0)
 The AESCTRDRBG instance must be reseeded. More...
 
#define AESCTRDRBG_STATUS_UNINSTANTIATED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 1)
 The AESCTRDRBG instance is uninstantiated. Close and reopen the instance. More...
 
#define AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 2)
 The operation does not support non-word-aligned input and/or output. More...
 
#define AESCTRDRBG_STATUS_KEYSTORE_ERROR   (AES_STATUS_KEYSTORE_GENERIC_ERROR)
 Importing generated key into KeyStore failed. More...
 
#define AESCTRDRBG_AES_BLOCK_SIZE_BYTES   16
 The AES block size in bytes. More...
 

Typedefs

typedef AESCommon_Config AESCTRDRBG_Config
 AESCTRDRBG Global configuration. More...
 
typedef AESCTRDRBG_ConfigAESCTRDRBG_Handle
 A handle that is returned from an AESCTRDRBG_open() call. More...
 

Enumerations

enum  AESCTRDRBG_AES_KEY_LENGTH { AESCTRDRBG_AES_KEY_LENGTH_128 = 16, AESCTRDRBG_AES_KEY_LENGTH_256 = 32 }
 Length in bytes of the internal AES key used by an instance. More...
 
enum  AESCTRDRBG_SEED_LENGTH { AESCTRDRBG_SEED_LENGTH_AES_128 = AESCTRDRBG_AES_KEY_LENGTH_128 + 16, AESCTRDRBG_SEED_LENGTH_AES_256 = AESCTRDRBG_AES_KEY_LENGTH_256 + 16 }
 Length in bytes of seed used to instantiate or reseed instance. More...
 
enum  AESCTRDRBG_ReturnBehavior { AESCTRDRBG_RETURN_BEHAVIOR_BLOCKING = AESCTR_RETURN_BEHAVIOR_BLOCKING, AESCTRDRBG_RETURN_BEHAVIOR_POLLING = AESCTR_RETURN_BEHAVIOR_POLLING }
 The way in which AESCTRDRBG function calls return after generating the requested entropy. More...
 

Functions

void AESCTRDRBG_init (void)
 This function initializes the AESCTRDRBG driver. More...
 
void AESCTRDRBG_Params_init (AESCTRDRBG_Params *params)
 Function to initialize the AESCTRDRBG_Params struct to its defaults. More...
 
AESCTRDRBG_Handle AESCTRDRBG_open (uint_least8_t index, const AESCTRDRBG_Params *params)
 This function opens a given AESCTRDRBG instance. More...
 
void AESCTRDRBG_close (AESCTRDRBG_Handle handle)
 Function to close an AESCTRDRBG instance specified by the AESCTRDRBG_Handle. More...
 
int_fast16_t AESCTRDRBG_getBytes (AESCTRDRBG_Handle handle, CryptoKey *randomBytes)
 Generates the requested number of random bytes. More...
 
int_fast16_t AESCTRDRBG_generateKey (AESCTRDRBG_Handle handle, CryptoKey *randomKey)
 Populates the provided CryptoKey object's plaintext key-material with random bytes. More...
 
int_fast16_t AESCTRDRBG_getRandomBytes (AESCTRDRBG_Handle handle, void *randomBytes, size_t randomBytesSize)
 Generates the requested number of random bytes and outputs to the given array. More...
 
int_fast16_t AESCTRDRBG_reseed (AESCTRDRBG_Handle handle, const void *seed, const void *additionalData, size_t additionalDataLength)
 Reseed an AESCTRDRBG instance. More...
 
AESCTRDRBG_Handle AESCTRDRBG_construct (AESCTRDRBG_Config *config, const AESCTRDRBG_Params *params)
 Constructs a new AESCTRDRBG object. More...
 

Variables

const AESCTRDRBG_Params AESCTRDRBG_defaultParams
 Default AESCTRDRBG_Params structure. More...
 

Macro Definition Documentation

§ AESCTRDRBG_STATUS_RESERVED

#define AESCTRDRBG_STATUS_RESERVED   AES_STATUS_RESERVED

Common AESCTRDRBG status code reservation offset. AESCTRDRBG driver implementations should offset status codes with AESCTRDRBG_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define AESCTRDRBGXYZ_STATUS_ERROR0 AESCTRDRBG_STATUS_RESERVED - 0
#define AESCTRDRBGXYZ_STATUS_ERROR1 AESCTRDRBG_STATUS_RESERVED - 1
#define AESCTRDRBGXYZ_STATUS_ERROR2 AESCTRDRBG_STATUS_RESERVED - 2

§ AESCTRDRBG_STATUS_SUCCESS

#define AESCTRDRBG_STATUS_SUCCESS   AES_STATUS_SUCCESS

Successful status code.

Functions return AESCTRDRBG_STATUS_SUCCESS if the function was executed successfully.

§ AESCTRDRBG_STATUS_ERROR

#define AESCTRDRBG_STATUS_ERROR   AES_STATUS_ERROR

Generic error status code.

Functions return AESCTRDRBG_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.

§ AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLE

#define AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE

An error status code returned if the hardware or software resource is currently unavailable.

AESCTRDRBG driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ AESCTRDRBG_STATUS_RESEED_REQUIRED

#define AESCTRDRBG_STATUS_RESEED_REQUIRED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 0)

The AESCTRDRBG instance must be reseeded.

An AESCTRDRBG instance may only service a limited number of bit generation requests before reseeding with more entropy is required.

§ AESCTRDRBG_STATUS_UNINSTANTIATED

#define AESCTRDRBG_STATUS_UNINSTANTIATED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 1)

The AESCTRDRBG instance is uninstantiated. Close and reopen the instance.

§ AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTED

#define AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTED   (AES_STATUS_DRIVER_SPECIFIC_ERROR - 2)

The operation does not support non-word-aligned input and/or output.

AESCTR driver implementations used by AESCTRDRBG may have restrictions on the alignment of input/output data due to performance limitations of the hardware.

§ AESCTRDRBG_STATUS_KEYSTORE_ERROR

#define AESCTRDRBG_STATUS_KEYSTORE_ERROR   (AES_STATUS_KEYSTORE_GENERIC_ERROR)

Importing generated key into KeyStore failed.

Functions return AESCTRDRBG_STATUS_KEYSTORE_ERROR if the KeyStore_PSA_importKey() did not return KEYSTORE_PSA_STATUS_SUCCESS

§ AESCTRDRBG_AES_BLOCK_SIZE_BYTES

#define AESCTRDRBG_AES_BLOCK_SIZE_BYTES   16

The AES block size in bytes.

Typedef Documentation

§ AESCTRDRBG_Config

AESCTRDRBG Global configuration.

The AESCTRDRBG_Config structure contains a set of pointers used to characterize the AESCTRDRBG driver implementation.

This structure needs to be defined before calling AESCTRDRBG_init() and it must not be changed thereafter.

See also
AESCTRDRBG_init()

§ AESCTRDRBG_Handle

A handle that is returned from an AESCTRDRBG_open() call.

Enumeration Type Documentation

§ AESCTRDRBG_AES_KEY_LENGTH

Length in bytes of the internal AES key used by an instance.

Enumerator
AESCTRDRBG_AES_KEY_LENGTH_128 
AESCTRDRBG_AES_KEY_LENGTH_256 

§ AESCTRDRBG_SEED_LENGTH

Length in bytes of seed used to instantiate or reseed instance.

Enumerator
AESCTRDRBG_SEED_LENGTH_AES_128 
AESCTRDRBG_SEED_LENGTH_AES_256 

§ AESCTRDRBG_ReturnBehavior

The way in which AESCTRDRBG function calls return after generating the requested entropy.

Not all AESCTRDRBG operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

AESCTRDRBG functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
AESCTRDRBG_RETURN_BEHAVIOR_BLOCKING X
AESCTRDRBG_RETURN_BEHAVIOR_POLLING X X X
Enumerator
AESCTRDRBG_RETURN_BEHAVIOR_BLOCKING 

The function call will block while AESCTRDRBG operation goes on in the background. AESCTRDRBG operation results are available after the function returns.The function call will continuously poll a flag while AESCTRDRBG operation goes on in the background. AESCTRDRBG operation results are available after the function returns.

AESCTRDRBG_RETURN_BEHAVIOR_POLLING 

Function Documentation

§ AESCTRDRBG_init()

void AESCTRDRBG_init ( void  )

This function initializes the AESCTRDRBG driver.

Precondition
The AESCTRDRBG_Config structure must exist and be persistent before this function can be called. This function must also be called before any other AESCTRDRBG driver APIs. This function call does not modify any peripheral registers.

§ AESCTRDRBG_Params_init()

void AESCTRDRBG_Params_init ( AESCTRDRBG_Params params)

Function to initialize the AESCTRDRBG_Params struct to its defaults.

Parameters
[out]paramsPointer to AESCTRDRBG_Params structure for initialization

§ AESCTRDRBG_open()

AESCTRDRBG_Handle AESCTRDRBG_open ( uint_least8_t  index,
const AESCTRDRBG_Params params 
)

This function opens a given AESCTRDRBG instance.

Precondition
AESCTRDRBG controller has been initialized using AESCTRDRBG_init()
Parameters
[in]indexLogical peripheral number for the AESCTRDRBG indexed into the AESCTRDRBG_Config table
[in]paramsPointer to an parameter block, if NULL it will use default values.
Returns
An AESCTRDRBG_Handle on success or a NULL on an error or if it has been opened already.
See also
AESCTRDRBG_init()
AESCTRDRBG_close()

§ AESCTRDRBG_close()

void AESCTRDRBG_close ( AESCTRDRBG_Handle  handle)

Function to close an AESCTRDRBG instance specified by the AESCTRDRBG_Handle.

Precondition
AESCTRDRBG_open() has to be called first.
Parameters
[in]handleAn AESCTRDRBG_Handle returned from AESCTRDRBG_open()
See also
AESCTRDRBG_open()

§ AESCTRDRBG_getBytes()

int_fast16_t AESCTRDRBG_getBytes ( AESCTRDRBG_Handle  handle,
CryptoKey randomBytes 
)

Generates the requested number of random bytes.

Deprecated:
This function has been replaced by a pair of new functions. See AESCTRDRBG_generateKey() and AESCTRDRBG_getRandomBytes().
Parameters
[in]handleAn AESCTRDRBG_Handle returned from AESCTRDRBG_open()
[in,out]randomBytesPointer to a CryptoKey object that should be already initialized to hold a plaintext key, provided with the length and the address of the plaintext key-material where the generated random bytes will be populated. Some implementations may require key-material to be word-aligned.
Return values
AESCTRDRBG_STATUS_SUCCESSRandom bytes generated.
AESCTRDRBG_STATUS_ERRORGeneric driver error. Random bytes not generated.
AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLEThe required hardware was unavailable. Random bytes not generated.
AESCTRDRBG_STATUS_RESEED_REQUIREDReseed counter >= reseed limit. Reseed required. Random bytes not generated.
AESCTRDRBG_STATUS_UNINSTANTIATEDDRBG uninstantiated. Close and reopen the instance with fresh seed. Random bytes not generated.
AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTEDPointer to randomBytes key material must be word-aligned.

§ AESCTRDRBG_generateKey()

int_fast16_t AESCTRDRBG_generateKey ( AESCTRDRBG_Handle  handle,
CryptoKey randomKey 
)

Populates the provided CryptoKey object's plaintext key-material with random bytes.

Note
This function replaces AESCTRDRBG_getBytes(). See AESCTRDRBG_getRandomBytes() to output random bytes to an array instead.
Parameters
[in]handleAn AESCTRDRBG_Handle returned from AESCTRDRBG_open()
[in,out]randomKeyPointer to a CryptoKey object that should be already initialized to hold a plaintext key, provided with the length and the address of the plaintext key-material where the generated random bytes will be populated. Some implementations may require key-material to be word-aligned.
Return values
AESCTRDRBG_STATUS_SUCCESSKey-material generated.
AESCTRDRBG_STATUS_ERRORGeneric driver error. Key-material not generated.
AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLEThe required hardware was unavailable. Key-material not generated.
AESCTRDRBG_STATUS_RESEED_REQUIREDReseed counter >= reseed limit. Reseed required. Key-material not generated.
AESCTRDRBG_STATUS_UNINSTANTIATEDDRBG uninstantiated. Close and reopen the instance with fresh seed. Key-material not generated.
AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTEDPointer to randomKey key material must be word-aligned.

§ AESCTRDRBG_getRandomBytes()

int_fast16_t AESCTRDRBG_getRandomBytes ( AESCTRDRBG_Handle  handle,
void *  randomBytes,
size_t  randomBytesSize 
)

Generates the requested number of random bytes and outputs to the given array.

Attention
This function should not be confused with the deprecated AESCTRDRBG_getBytes(). AESCTRDRBG_getBytes() output random bytes to a CryptoKey while this new function outputs random bytes to an array.
Note
See AESCTRDRBG_generateKey() to output random bytes to a CryptoKey instead.
Parameters
[in]handleAn AESCTRDRBG_Handle returned from AESCTRDRBG_open()
[out]randomBytesA pointer to an array that stores the random bytes output by this function. Some implementations may require this array to be word-aligned.
[in]randomBytesSizeThe size in bytes of the random data required.
Return values
AESCTRDRBG_STATUS_SUCCESSRandom bytes generated.
AESCTRDRBG_STATUS_ERRORGeneric driver error. Random bytes not generated.
AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLEThe required hardware was unavailable. Random bytes not generated.
AESCTRDRBG_STATUS_RESEED_REQUIREDReseed counter >= reseed limit. Reseed required. Random bytes not generated.
AESCTRDRBG_STATUS_UNINSTANTIATEDDRBG uninstantiated. Close and reopen the instance with fresh seed. Random bytes not generated.
AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTEDPointer to randomBytes array must be word-aligned.

§ AESCTRDRBG_reseed()

int_fast16_t AESCTRDRBG_reseed ( AESCTRDRBG_Handle  handle,
const void *  seed,
const void *  additionalData,
size_t  additionalDataLength 
)

Reseed an AESCTRDRBG instance.

Parameters
[in]handleAn AESCTRDRBG_Handle returned from AESCTRDRBG_open()
[in]seedEntropy to mix into the AESCTRDRBG instance state
[in]additionalDataOptional non-secret additional data to mix into the instance state.
[in]additionalDataLengthLength of the optional additional data. 0 <= additionalDataLength <= seed length of the instance.
Return values
AESCTRDRBG_STATUS_SUCCESSReseed successful. Reseed counter reset.
AESCTRDRBG_STATUS_ERRORReseed not successful. Reseed counter not reset.
AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLEThe requires hardware was unavailable.
AESCTRDRBG_STATUS_UNINSTANTIATEDDRBG uninstantiated. Close and reopen the instance with fresh seed.

§ AESCTRDRBG_construct()

AESCTRDRBG_Handle AESCTRDRBG_construct ( AESCTRDRBG_Config config,
const AESCTRDRBG_Params params 
)

Constructs a new AESCTRDRBG object.

Unlike AESCTRDRBG_open(), AESCTRDRBG_construct() does not require the hwAttrs and object to be allocated in a AESCTRDRBG_Config array that is indexed into. Instead, the AESCTRDRBG_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configAESCTRDRBG_Config describing the location of the object and hwAttrs.
paramsAESCTRDRBG_Params to configure the driver instance.
Returns
Returns an AESCTRDRBG_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ AESCTRDRBG_defaultParams

const AESCTRDRBG_Params AESCTRDRBG_defaultParams

Default AESCTRDRBG_Params structure.

See also
AESCTRDRBG_Params_init()
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale