Flash

The flash is split into erasable pages of 8 kB. The various sections of flash and their associate linker files are as follows.

  • Flash Reset Vector Table: This table holds the first 16 reset vectors that are critical for booting up the device. These vectors are set at build time and cannot be dynamically changed. See sec-flash-vector-table for more information.

  • Non-volatile (NV) Area: used for nonvolatile memory storage by the Zigbee network information and also available for use by the application. See Non-Volatile Memory Items for configuring NV.

  • Application and Stack Image Code Space: A single region that contains both application and stack code in flash. This image is configured in the linker configuration file of the application: <device name>_app_and_stack.icf (IAR) and <device name>_app.cmd (CCS).

Non-Volatile Storage Architecture

This section will describe the non volatile storage system that is implemented and used on the CC13xx or CC26xx. This system provides access to non volatile storage that can be safely shared between the user application and the protocol stack.

The system has the following properties and offers the following features:

  • Thread safe access to non volatile memory

  • ID based system that decouples a storage item from its address in memory

  • Space efficient storage with automatic compaction

  • Power loss tolerant data preservation

The implementation of this software system relies on several layers which are illustrated below.

../_images/ditaa-d54ad0c27042b56ccadd5e15b9895c3895a91080.png

Non Volatile Interface (NVINTF)

The NVINTF is an abstraction layer that defines a common set of APIs for interacting with non volatile memory using a ID system. This common set of APIs allow for new methods of NV storage to be implemented without changing the API calls in the stack and application. The ID system is most efficient because it decouples the data stored from its address in flash. This is necessary because flash banks must have the entire sector erased before writing again. (with the exception of clearing a bit). Using the ID system, when an NV item needs to be updated, it can simply be invalidated and stored again at a different address. Once the NV system becomes full of unused items, a compaction will occur. A compaction is the removal of unused items.

The NVINTF is function pointer based, each underlying transport must plug a function table and provide an implementation for the common set of APIs.

This interface is defined in nvintf.h. The NVINTF is not intended to be changed by the customer, but instead used as is.

Non Volatile On-Chip Multi Page (NVOCMP) Driver

The NVOCMP driver implements a non-volatile memory system that utilizes multiple consecutive pages of on-chip Flash memory. After initialization, all pages except one are “active” and the remaining one page is available for “compaction” when the active pages do not have enough empty space for data write operation. Compaction can occur “just in time” during a data write operation or “on demand” by application request. The compaction process is designed to survive a power cycle before it completes. It will resume where it was interrupted and complete the process. The number of NV pages can be set by the NVOCMP_NVPAGES preprocessor define. If this is not set, it will default to 2.

Each flash page contains a “page header” which indicates its current state. The page header is located at the first byte of the flash page. Following the page header is the “compact header”, which indicates the flash page’s compaction state. The remainder of the flash page contains NV data items which are packed together following the page header and compact header.

Each NV data item is unique and has two parts:

  1. A data block which is stored first (lower memory address)

  2. An item header following the data block (higher memory address)

The item header (defined by NVOCMP_itemHdr_t) contains status information required to traverse packed data items in the flash page. An example of the NV item memory layout storing a single byte of data is illustrated below.

../_images/nvintf_header.png

NV Item Header:

Field

Size (bits)

Purpose

System ID

6

Indicates the system component identifier

Item ID

10

Indicates the item data identifier

Sub ID

10

Identifier of the sub-data related to the NV item

Length

12

Length of the data block

CRC

8

CRC value of NV item

Status Bits

2

Indicates CRC integrity and if item is active

Signature

8

Used to detect presence of a NV item in flash

For each NV item that is added or updated in NV storage, the item is written to the next lowest available memory address in the active flash page. If the NV item is being updated, the old NV item will be marked as inactive. Inactive items are removed from memory when a memory compaction takes place.

For more information, see the API documentation in nvocmp.h and the design description in nvocmp.c.

Non Volatile Storage (NVS) Driver

The NVS driver provides reentrant functions for writing to and reading from flash. It also provides a common interface to both internal and external flash. More information can be found in the TI Drivers documentation. The stack will use internal NV, currently this is all that is supported.

Non-Volatile Memory Items

Global Configuration Non-Volatile Memory

Global device configuration items are stored in zglobals.c. This includes items such as PAN ID, key information, network settings, etc. The default values for most of these items are specified in SysConfig. These items are loaded to RAM at startup for quick access during Z-Stack operation. To initialize the non-volatile memory area to store these items, the compile flag NV_INIT must be enabled in your project (it is enabled by default in the sample applications).

Network Layer Non-Volatile Memory

A Zigbee device has lots of state information that needs to be stored in non-volatile memory so that it can be recovered in case of an accidental reset or power loss. Otherwise, it will not be able to rejoin the network or function effectively.

This feature is enabled by default by the inclusion of the NV_RESTORE compile option. Note that this feature must be always enabled in a real Zigbee network. The ability to disable it is only intended for use in the development stage.

The ZDO layer is responsible for the saving and restoring of the Network Layer’s vital information, but it is the BDB layer which will define when to retrieve this information or when to clear and start as a “factory new” device. This includes the Network Information Base (NIB - Attributes required to manage the network layer of the device); the list of child and parent devices; and the table containing the application bindings. This is also used for security to store frame counters and keys.

Upon reset, if the device is not meant to return to its factory new state, then it will use this information to restore itself in the network.

Upon initializing, the BDB layer will check the attribute if this device was commissioned to a network (bdbNodeIsOnANetwork). If it was commissioned to a network and it was also instructed to resume operations in the same network, then the BDB layer will call ZDOInitDeviceEx(), which will handle the resume operation according to the state and the logical device type.

Application Non-Volatile Memory

In general, a device must have non-volatile memory enabled to be certified, because it must remember its network configuration. In addition to the stack ‘internal’ data, the NVM can also be used to store application data.

Reading and writing to NV is done using the NV functions contained within zstack_user0Cfg.nvFps. The sample applications have access to these functions via the global static NVINTF_nvFuncts_t *pfnZdlNV = NULL;

The NV area of flash is used for storing persistent data for the application. For more information on the NV On-Chip Multi-Page (NVOCMP) driver please refer to nvocmp.c which describes the implementation details of the multi-page NV and lists the maximum values of custom NV IDs available to the applications as such:

// Maximum ID parameters - must be coordinated with header compression,
// Increasing these limits requires modification of the readHdr() function
#define NVOCMP_MAXSYSID   0x003F  //  6 bits
#define NVOCMP_MAXITEMID  0x03FF  // 10 bits
#define NVOCMP_MAXSUBID   0x03FF  // 10 bits
#define NVOCMP_MAXLEN     0x03FF  // 10 bits

The last page in flash is the CCA page, the pages before that are reserved for the NV area as defined by NVOCMP_NVPAGES. The example projects use the NV driver with the API defined in nvintf.h. The NV driver is set up in main.c:

#ifdef NV_RESTORE
    /* Setup the NV driver */
    NVOCMP_loadApiPtrs(&zstack_user0Cfg.nvFps);

    if(zstack_user0Cfg.nvFps.initNV)
    {
        zstack_user0Cfg.nvFps.initNV( NULL);
    }
#endif

Then the applications use the function pointers in zstack_user0Cfg to call the NV functions defined in nvintf.h:

//! Structure of NV API function pointers
typedef struct nvintf_nvfuncts_t
{
    //! Initialization function
    NVINTF_initNV initNV;
    //! Compact NV function
    NVINTF_compactNV compactNV;
    //! Create item function
    NVINTF_createItem createItem;
    //! Delete NV item function
    NVINTF_deleteItem deleteItem;
    //! Read item function
    NVINTF_readItem readItem;
    //! Write item function
    NVINTF_writeItem writeItem;
    //! Write existing item function
    NVINTF_writeItemEx writeItemEx;
    //! Get item length function
    NVINTF_getItemLen getItemLen;
} NVINTF_nvFuncts_t;

The following is an example of NV memory registration from zcl_sampledoorlock.c:

void sampleApp_task(NVINTF_nvFuncts_t *pfnNV)
{
  // Save and register the function pointers to the NV drivers
  pfnZdlNV = pfnNV;
  zclport_registerNV(pfnZdlNV, ZCL_PORT_SCENE_TABLE_NV_ID);

  // Initialize application
  zclSampleDoorLock_initialization();

  // No return from task process
  zclSampleDoorLock_process_loop();
}

The following is an example of a NV read from zclSampleDoorLock_Init of zcl_sampledoorlock.c:

// Initialize NVM for storing PIN information
if(pfnZdlNV)
{
    NVINTF_itemID_t nvId;
    uint32_t nvErr = NVINTF_NOTFOUND;

    // Fill in the NV ID header
    nvId.systemID = NVINTF_SYSID_APP;
    nvId.itemID = (uint16_t)DLSAPP_NV_DOORLOCK_PIN;
    nvId.subID = (uint16_t)0;

    // Read the PIN from NV
    if(pfnZdlNV->readItem)
    {
        nvErr = pfnZdlNV->readItem(nvId, 0, DLSAPP_NV_DOORLOCK_PIN_LEN,
                                   aiDoorLockMasterPINCode);
    }

    // If the PIN doesn't exist in NV, create it
    if((nvErr == NVINTF_NOTFOUND) && pfnZdlNV->createItem)
    {
        pfnZdlNV->createItem(nvId, DLSAPP_NV_DOORLOCK_PIN_LEN,
                             aiDoorLockMasterPINCode);
    }
}

The following is an example of a NV write from zclSampleDoorLock_UiActionChangePin of zcl_sampledoorlock.c:

if(pfnZdlNV && pfnZdlNV->writeItem)
{
    NVINTF_itemID_t nvId;

    nvId.systemID = NVINTF_SYSID_APP;
    nvId.itemID = (uint16_t)DLSAPP_NV_DOORLOCK_PIN;
    nvId.subID = (uint16_t)0;

    pfnZdlNV->writeItemEx(nvId, 0, DLSAPP_NV_DOORLOCK_PIN_LEN,
                          aiDoorLockMasterPINCode);
}

The NV system is a collection of NV items. Each item is unique and have the following pieces to it (defined in nvintf.h):

/**
*  NV Item Identification structure
*/

typedef struct nvintf_itemid_t
{
    //! NV System ID - identifies system (ZStack, BLE, App, OAD...)
    uint8_t systemID;
    //! NV Item ID
    uint16_t itemID;
    //! NV Item sub ID
    uint16_t subID;
} NVINTF_itemID_t;

Note

If migrating a project from Z-Stack 3.4.0 or earlier to 3.5.0 or later, ZSTACK_NVOCMP_MIGRATION must be defined in the 3.5.0+ project in order to compensate for the changes involved with upgrading from the NVOCTP to the NVOCMP driver. This only applies to field upgrades where no factory reset is intended so that the NV memory is retained in order to keep network settings. The values modified in zgUpgradeNvDriver should not change size between versions or else zgUpgradeNvDriver itself will need to be altered to accomodate. These include:

  • ZDSECMGR_TC_DEVICE_MAX

  • ZDSECMGR_TC_DEVICE_IC_MAX

  • ZDSECMGR_ENTRY_MAX

  • MAX_NWK_SEC_MATERIAL_TABLE_ENTRIES

  • GPP_MAX_PROXY_TABLE_ENTRIES

  • GPS_MAX_SINK_TABLE_ENTRIES

Note

If using APS groups and upgrading a project from Z-Stack 4.4.0 or earlier to 5.1.0 or later using the OTA method, ZSTACK_NVOCMP_MIGRATION must be defined in the 5.1.0+ project to account for a new feature in which each group table has been separated into its own NV ID subset.

Likewise, for upgrading from Z-Stack 5.2.0-, ZSTACK_5_30_NV_MIGRATION and ZSTACK_NV_FORMAT_UPDATE need to be defined for the 5.3.0+ project due to the new format of TCLK items. If upgrading from Z-Stack 3.4.0- or using APS groups with Z-Stack 4.4.0-, then incremental upgrades are necessary to transition between all of the required changes.

Non-Volatile Memory Low Voltage Detection

Z-Stack utilizes the on-chip battery monitor to make sure the device’s power level is above a given theshold before writing contents to the NV memory. This prevents flash memory corruption during low voltage operation. The aforementioned detection threshold is determined by NVOCMP_MIN_VDD_FLASH_MV and is represented in units of millivolts. A value of at least 2000 is recommended for typical Z-Stack applications. If any NV operations are prevented due to this feature then the application can be notified by a callback such as Main_lowVoltageCb used in main.c of the Z-Stack sample applications:

/*!
 * @brief       Callback function when voltage is lower than NVOCMP_MIN_VDD_FLASH_MV
 *              during an NV write operation
 *
 * @param       voltage - Measured device voltage
 */
#ifdef NVOCMP_MIN_VDD_FLASH_MV
void Main_lowVoltageCb(uint32_t voltage)
{
    /* Implement any safety precautions for application due to low voltage detected */
}
#endif

Modifying Non-Volatile Memory Allocation

By default, Z-Stack projects allocate two flash pages for non-volatile (NV) memory with the pre-define NVOCMP_NVPAGES=2. This is located in the Projects Properties’ BuildArm CompilerPredefined Symbols as well as BuildArm LinkerAdvanced OptionsCommand File Preprocessing and the value from both locations should always match. The purpose of these definitions is to allow one dedicated page for compaction and other pages for storage. In some use cases, for example a Zigbee Coordinator Trust Center with a large number of devices connected (see Network Configurations for applicable changes), it may be necessary to increase the number of NV storage pages. Users will also need to modify the aforementioned NVOCMP_NVPAGES=2 locations along with Region Base and Region Size settings in the project’s .syscfg file TI DriversNVSInternal Flash. The command linker (.cmd) file accounts for changes automatically:

#ifndef NVOCMP_NVPAGES
#define NVOCMP_NVPAGES 2
#endif

#define FLASH_BASE 0x00000000
#define FLASH_SIZE (0x56000 - (NVOCMP_NVPAGES * 0x2000))
#define FLASH_NV_BASE (0x56000 - (NVOCMP_NVPAGES * 0x2000))
#define FLASH_NV_SIZE (NVOCMP_NVPAGES * 0x2000)
#define FLASH_LAST_BASE 0x56000
#define FLASH_LAST_SIZE 0x2000

For example, if NVOCMP_NVPAGES was increased to three (two pages for storage and one for compaction) then FLASH_SIZE, FLASH_NV_BASE, and Region Base would decrease to 0x50000 and FLASH_NV_SIZE and Region Size would increase to 0x6000 (since one page of flash is 0x2000 bytes).

The amount of required NV memory greatly depends on the definitions provided in the table below. Total NV allocation required for a Z-Stack project can be estimated by multiplying the bytes per entry by the value of the definition then adding them all together along with ~2.3 kB for remaining NV items which aren’t as liable to fluctuate depending on network settings.

Definition

Bytes per entry

Default value

NWK_MAX_DEVICE_LIST

23

20

ZDSECMGR_TC_DEVICE_MAX

27

40

NWK_MAX_ADDRESSES

19

70

Note

The maximum value of NVOCMP_NVPAGES allowed is five, which equals one compaction page (0x2000 bytes) and four storage pages (0x8000 bytes).

For IAR projects the user does not have to modify the linker command (.icf) file. The required sizes will be calculated by the compiler.