Z-Stack API Reference  6.30.00.23
_zstack_devicetypes_t Struct Reference

#include <zstack.h>

Data Fields

bool coodinator
 True if device is capable of being a coordinator.
 
bool router
 True if device is capable of being a router.
 
bool enddevice
 True if device is capable of being an end device.
 

Detailed Description

Device type capable information, a device can be capable of one or more of these types.


The documentation for this struct was generated from the following file: