Z-Stack API Reference  6.30.00.23
_zstack_zdomgmtdirectjoinreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t nwkAddr
 
zstack_LongAddr_t deviceAddress
 
zstack_CapabilityInfo_t capInfo
 

Detailed Description

Structure to send a ZDO Mgmt Direct Join Request.

Field Documentation

§ capInfo

MAC capabilities

§ deviceAddress

zstack_LongAddr_t deviceAddress

64 bit IEEE address of the device to be joined to nwkAddr

§ nwkAddr

uint16_t nwkAddr

Targeted device


The documentation for this struct was generated from the following file: