![]() |
![]() |
Z-Stack API Reference
6.30.00.23
|
#include <zstack.h>
Data Fields | |
uint16_t | srcAddr |
zstack_ZdpStatus | status |
uint32_t | scannedChannels |
uint16_t | totalTrans |
uint16_t | transFails |
uint8_t | n_energyValuesList |
uint8_t * | pEnergyValuesList |
Structure to send a ZDO Mgmt Network Update Notify Indication.
uint8_t n_energyValuesList |
Number of items in the energyValuesList
uint8_t* pEnergyValuesList |
Array of bytes, each representing the energy value for each scanned channel
uint32_t scannedChannels |
Bitmap - list of channels scanned by the request.
uint16_t srcAddr |
Source Address
zstack_ZdpStatus status |
Response Status
uint16_t totalTrans |
Count of the total transmissions
uint16_t transFails |
Sum of the total transmission failures