Z-Stack API Reference  6.30.00.23
zclGpPairing_t Struct Reference

Data Fields

afAddrType_t * srcAddr
 Local device address.
 
uint8_t wasBroadcast
 
uint8_t options [3]
 TRUE if network destination was a broadcast address. More...
 
uint8_t * pData
 Pairing command payload.
 

Field Documentation

§ options

uint8_t options[3]

TRUE if network destination was a broadcast address.

Pairing options bitfield.


The documentation for this struct was generated from the following file: