Z-Stack API Reference  6.30.00.23
zclOTA_QuerySpecificFileReqParams_t Struct Reference

Data Fields

uint8_t nodeAddr [Z_EXTADDR_LEN]
 This is the IEEE address of the client device.
 
zclOTA_FileID_t fileId
 File Id structure.
 
uint16_t stackVersion
 Stack version value.
 

The documentation for this struct was generated from the following file: