Data Structures | Macros | Typedefs | Functions
Power.h File Reference

Detailed Description

Power Manager.


Overview

The Power Manager facilitates the transition of the MCU from active states to sleep states and vice versa. It provides other drivers the ability to set and release dependencies on hardware resources, and keeps reference counts on each resource to know when to enable or disable the resource. It provides drivers the ability to register callback functions to be invoked upon specific power events. In addition, drivers and applications can set or release constraints to prevent the MCU from transitioning into specific active or sleep states. Refer to the device specific power driver header file device specific information.


Usage

This documentation provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the APIs are provided in subsequent sections.

Synopsis

Note
The following example demonstrates usage of some of the Power driver APIs.This example is intended for reference only and is not intended for application use. You should refer to the device specific Power driver header for valid API usage and arguments.
// Import Power Driver definitions
// One-time initialization of Power manager
// Set power dependency on a resource
status = Power_setDependency(resourceId);
if (status != Power_SOK) {
// Error occurred
}
// Set a power constraint
status = Power_setConstraint(constraintId);
if (status != Power_SOK) {
// Error occurred
}
// Other application code
// Release a previously set power constraint
status = Power_releaseConstraint(constraintId);
if (status != Power_SOK) {
// Error occurred
}
status = Power_releaseDependency(resourceId);
if (status != Power_SOK) {
// Error occurred
}

Examples

Note
The following examples are intended for reference only and are not intended for application use. You should refer to the device specific Power driver header file for more usage information.

Enabling Power Policy

// Import Power Driver definitions
// One-time initialization of Power manager
// Enable power policy

Disabling Power Policy

// Import Power Driver definitions
bool flag;
// One-time initialization of Power manager
// Disable power policy
if (flag == false) {
// Power policy was already disabled
}

Using Power Constraints

// Import Power Driver definitions
uint32_t mask;
int16_t status;
// One-time initialization of Power manager
// Set a power constraint
status = Power_setConstraint(constraintId);
if (status != Power_SOK) {
// Error occurred setting constraint
}
// Read mask of currently set power constraints
// Release previously set constraint
status = Power_releaseConstraint(constraintId);
if (status != Power_SOK) {
// Error occurred releasing constraint
}

Using Power Dependency

// Import Power Driver definitions
int16_t count;
int16_t status;
// One-time initialization of Power manager
// Set a power dependency
status = Power_setDependency(resourceId);
if (status != Power_SOK) {
// Error occurred setting dependency
}
// Get the dependency count of the resource
count = Power_getDependencyCount(resourceId);
if (count == Power_EINVALIDINPUT) {
// Invalid resourceId used
}
if (count > 0) {
// At least 1 dependency exists for the resource.
// Regardless, we may safely release the dependency when we
// no longer need the resource.
}
// Release a power dependency
status = Power_releaseDependency(resourceId);
if (status != Power_SOK) {
// Error occurred releasing dependency
}

Using Power Notify

The application must define a Power_NotifyFxn function and allocate memory for the Power_NotifyObj object.

// Import Power Driver definitions
// Application Power_NotifyObj object
Power_NotifyObj powerNotifyObj;
// Application Power_NotifyFxn function prototype
static int postNotifyFxn(unsigned int eventType, uintptr_t eventArg,
uintptr_t clientArg);

The application must register for the event. Here, we use pseudo event names. You should refer to the device specific power driver header file for eventTypes. Inside the infinite loop, we wait for a semaphore to be post from our notification callback.

// Application thread
void thread(void)
{
int16_t status;
unsigned int eventTypes = LOW_POWER_EXIT | LOW_POWER_ENTER;
uintptr_t clientArg = semaphoreHandle;
status = Power_registerNotify(&powerNotifyObj, eventTypes,
postNotifyFxn, clientArg);
while (1)
{
sem_wait(semaphoreHandle);
// Do something
// Unregister for the notification. After this call,
// our postNotifyFxn() will never be called again unless
// we use Power_registerNotify() again.
Power_unregisterNotify(&powerNotifyObj);
break;
}
}

The application may implement the power notify function to fit their needs. The Power_NotifyFxn should always return Power_NOTIFYDONE or Power_NOTIFYERROR.

// Application Power_NotifyFxn function implementation
static int postNotifyFxn(unsigned int eventType, uintptr_t eventArg,
uintptr_t clientArg)
{
sem_t semaphoreHandle = (sem_t) clientArg;
if (eventType == LOW_POWER_EXIT) {
sem_post(semaphoreHandle);
return (Power_NOTIFYDONE);
}
if (eventType == LOW_POWER_ENTER) {
// Store something in RAM
return (Power_NOTIFYDONE);
}
// We received an unexpected event type
}

Power transitions

// Import Power Driver definitions
uint32_t totalLatency, resumeLatency;
int16_t status;
// One-time initialization of Power manager
// Get the current power transition state
switch (status)
{
// No transitions in progress
break;
// Transition to sleep in progress
break;
// Transition from sleep in progress
break;
// Performance level change in progress
break;
}
// Get the Power_TOTAL and Power_RESUME transition latency for a
// device specific sleepState. Latency is in microseconds.
totalLatency = Power_getTransitionLatency(sleepState, Power_TOTAL);
resumeLatency = Power_getTransitionLatency(sleepState, Power_RESUME);

Configuration

Note
The Power Manager APIs and configuration parameters are described here. For a detailed description of terms and concepts, and usage by different types of software components (peripheral drivers, power policies, and applications) please see the SimpleLink SDK Power Management User's Guide.
#include <ti/drivers/utils/List.h>
Include dependency graph for Power.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Power_NotifyObj
 Power notify object structure. More...
 

Macros

#define Power_TOTAL   (1U)
 
#define Power_RESUME   (2U)
 
#define Power_NOTIFYDONE   (0)
 
#define Power_NOTIFYERROR   (-1)
 
#define Power_SOK   (0)
 
#define Power_EFAIL   (-1)
 
#define Power_EINVALIDINPUT   (-2)
 
#define Power_EINVALIDPOINTER   (-3)
 
#define Power_ECHANGE_NOT_ALLOWED   (-4)
 
#define Power_EBUSY   (-5)
 
#define Power_ACTIVE   (1U)
 
#define Power_ENTERING_SLEEP   (2U)
 
#define Power_EXITING_SLEEP   (3U)
 
#define Power_ENTERING_SHUTDOWN   (4U)
 
#define Power_CHANGING_PERF_LEVEL   (5U)
 

Typedefs

typedef void(* Power_PolicyInitFxn) (void)
 Power policy initialization function pointer. More...
 
typedef void(* Power_PolicyFxn) (void)
 Power policy function pointer. More...
 
typedef int_fast16_t(* Power_NotifyFxn) (uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg)
 Power notify callback function used with the Power_registerNotify() More...
 

Functions

bool Power_disablePolicy (void)
 Disable the configured power policy from running when the CPU is idle. More...
 
void Power_enablePolicy (void)
 Enable the configured power policy to run when the CPU is idle. More...
 
uint_fast32_t Power_getConstraintMask (void)
 Get the constraints that have been declared with Power. More...
 
int_fast16_t Power_getDependencyCount (uint_fast16_t resourceId)
 Get the current dependency count for a resource. More...
 
uint_fast16_t Power_getPerformanceLevel (void)
 Get the current performance level. More...
 
uint_fast32_t Power_getTransitionLatency (uint_fast16_t sleepState, uint_fast16_t type)
 Get the hardware transition latency for a sleep state. More...
 
uint_fast16_t Power_getTransitionState (void)
 Get the current transition state of the Power Manager. More...
 
void Power_idleFunc (void)
 Power function to be added to the application idle loop. More...
 
int_fast16_t Power_init (void)
 Power initialization function. More...
 
int_fast16_t Power_registerNotify (Power_NotifyObj *pNotifyObj, uint_fast16_t eventTypes, Power_NotifyFxn notifyFxn, uintptr_t clientArg)
 Register a function to be called upon a specific power event. More...
 
int_fast16_t Power_releaseConstraint (uint_fast16_t constraintId)
 Release a previously declared constraint. More...
 
int_fast16_t Power_releaseDependency (uint_fast16_t resourceId)
 Release a previously declared dependency. More...
 
void Power_reset (void)
 Resets the system and causes it to reboot. More...
 
int_fast16_t Power_setConstraint (uint_fast16_t constraintId)
 Declare an operational constraint. More...
 
int_fast16_t Power_setDependency (uint_fast16_t resourceId)
 Declare a dependency upon a resource. More...
 
int_fast16_t Power_setPerformanceLevel (uint_fast16_t level)
 Set the MCU performance level. More...
 
void Power_setPolicy (Power_PolicyFxn policy)
 Set a new Power policy. More...
 
int_fast16_t Power_shutdown (uint_fast16_t shutdownState, uint_fast32_t shutdownTime)
 Put the device into a shutdown state. More...
 
int_fast16_t Power_sleep (uint_fast16_t sleepState)
 Transition the device into a sleep state. More...
 
void Power_unregisterNotify (Power_NotifyObj *pNotifyObj)
 Unregister previously registered notifications. More...
 

Typedef Documentation

§ Power_PolicyInitFxn

typedef void(* Power_PolicyInitFxn) (void)

Power policy initialization function pointer.

§ Power_PolicyFxn

typedef void(* Power_PolicyFxn) (void)

Power policy function pointer.

§ Power_NotifyFxn

typedef int_fast16_t(* Power_NotifyFxn) (uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg)

Power notify callback function used with the Power_registerNotify()

Parameters
[in]eventTypeThe eventTypes parameter identifies the type of power event for which the notify callback function was called.
[in]eventArgAn optional eventType specific argument.
[in]clientArgPointer to a custom argument.
Return values
Power_NOTIFYDONEif the client processed the notification successfully
Power_NOTIFYERRORif an error occurred during notification.
See also
Power_registerNotify()
Power_unregisterNotify()
Power_NotifyObj
Using power notify

Function Documentation

§ Power_disablePolicy()

bool Power_disablePolicy ( void  )

Disable the configured power policy from running when the CPU is idle.

Calling this function clears the flag that controls whether the configured power policy function is invoked on each pass through the Idle loop. This function call will override both a 'true' setting of the "enablePolicy" setting in the Power Manager configuration object, as well as a previous runtime call to the Power_enablePolicy() function.

Returns
The old value of "enablePolicy".
See also
Power_enablePolicy()
Enabling power policy
Disabling power policy

§ Power_enablePolicy()

void Power_enablePolicy ( void  )

Enable the configured power policy to run when the CPU is idle.

Calling this function sets a flag that will cause the configured power policy function to be invoked on each pass through the Idle loop. This function call will override both a 'false' setting of the "enablePolicy" setting in the Power Manager configuration object, as well as a previous runtime call to the Power_disablePolicy() function.

For some processor families, automatic power transitions can make initial application development more difficult, as well as being at odds with basic debugger operation. This convenience function allows an application to be initially configured, built, and debugged, without automatic power transitions during idle time. When the application is found to be working, this function can be called (typically in main()) to enable the policy to run, without having to change the application configuration.

See also
Power_disablePolicy()
Enabling power policy
Disabling power policy

§ Power_getConstraintMask()

uint_fast32_t Power_getConstraintMask ( void  )

Get the constraints that have been declared with Power.

This function returns a bitmask indicating the constraints that are currently declared to the Power Manager (via previous calls to Power_setConstraint()). For each constraint that is currently declared, the corresponding bit in the bitmask will be set. For example, if two clients have independently declared two different constraints, the returned bitmask will have two bits set.

Constraint identifiers are device specific, and defined in the device-specific Power include file. For example, the constraints for MSP432 are defined in PowerMSP432.h. The corresponding bit in the bitmask returned by this function can be derived by a left-shift using the constraint identifier. For example, for MSP432, for the corresponding bit for the PowerMSP432_DISALLOW_SLEEP constraint, the bit position is determined by the operation: (1 << PowerMSP432_DISALLOW_SLEEP)

Returns
A bitmask of the currently declared constraints.
See also
Power_setConstraint()
Using power constraints

§ Power_getDependencyCount()

int_fast16_t Power_getDependencyCount ( uint_fast16_t  resourceId)

Get the current dependency count for a resource.

This function returns the number of dependencies that are currently declared upon a resource.

Resource identifiers are device specific, and defined in the device-specific Power include file. For example, the resources for CC32XX are defined in PowerCC32XX.h.

Parameters
[in]resourceIdresource id
Returns
The number of dependencies declared for the resource.
Return values
Power_EINVALIDINPUTif the resourceId is invalid or this function is not supported by the device specific implementation.
See also
Power_setDependency()
Using power dependency

§ Power_getPerformanceLevel()

uint_fast16_t Power_getPerformanceLevel ( void  )

Get the current performance level.

This function returns the current device performance level in effect.

If performance scaling is not supported for the device, this function will always indicate a performance level of zero.

Returns
The current performance level.
See also
Power_setPerformanceLevel()

§ Power_getTransitionLatency()

uint_fast32_t Power_getTransitionLatency ( uint_fast16_t  sleepState,
uint_fast16_t  type 
)

Get the hardware transition latency for a sleep state.

This function reports the minimal hardware transition latency for a specific sleep state. The reported latency is that for a direct transition, and does not include any additional latency that might occur due to software-based notifications.

Sleep states are device specific, and defined in the device-specific Power include file. For example, the sleep states for CC32XX are defined in PowerCC32XX.h.

This function is typically called by the power policy function. The latency is reported in units of microseconds.

Parameters
[in]sleepStatethe sleep state
[in]typePower_Latency_Type (Power_TOTAL or Power_RESUME)
Returns
The latency value, in units of microseconds.
See also
Power transitions

§ Power_getTransitionState()

uint_fast16_t Power_getTransitionState ( void  )

Get the current transition state of the Power Manager.

Returns
The current Power_Transition_State.
Return values
Power_ACTIVEreturned when no transitions are in progress.
Power_ENTERING_SLEEPreturned during the transition to sleep, before sleep has occurred.
Power_EXITING_SLEEPreturned after wakeup, as the device is being transitioned back to Power_ACTIVE.
Power_CHANGING_PERF_LEVELreturned when a change is being made to the performance level.
See also
Power transitions

§ Power_idleFunc()

void Power_idleFunc ( void  )

Power function to be added to the application idle loop.

This function should be added to the application idle loop. (The method to do this depends upon the operating system being used.) This function will invoke the configured power policy function when appropriate. The specific policy function to be invoked is configured as the 'policyFxn' in the application-defined Power configuration object.

§ Power_init()

int_fast16_t Power_init ( void  )

Power initialization function.

This function initializes Power Manager internal state.

Warning
The application is responsible for ensuring this function is called prior to any other Power API. Additionally, this function must be be called prior to any other TI-Driver's APIs. This function is normally called prior to any operating system initialization.
Returns
Power_SOK

§ Power_registerNotify()

int_fast16_t Power_registerNotify ( Power_NotifyObj pNotifyObj,
uint_fast16_t  eventTypes,
Power_NotifyFxn  notifyFxn,
uintptr_t  clientArg 
)

Register a function to be called upon a specific power event.

This function registers a function to be called when a Power event occurs. Registrations and the corresponding notifications are processed in first-in-first-out (FIFO) order. The function registered must behave as described later, below.

The pNotifyObj parameter is a pointer to a pre-allocated, opaque object that will be used by Power to support the notification. This object could be dynamically allocated, or declared as a global object. This function will properly initialized the object's fields as appropriate; the caller just needs to provide a pointer to this pre-existing object.

The eventTypes parameter identifies the type of power event(s) for which the notify function being registered is to be called. (Event identifiers are device specific, and defined in the device-specific Power include file. For example, the events for MSP432 are defined in PowerMSP432.h.) The eventTypes parameter for this function call is treated as a bitmask, so multiple event types can be registered at once, using a common callback function. For example, to call the specified notifyFxn when both the entering deepsleep and awake from deepsleep events occur, eventTypes should be specified as: PowerMSP432_ENTERING_DEEPSLEEP | PowerMSP432_AWAKE_DEEPSLEEP

The notifyFxn parameter specifies a callback function to be called when the specified Power event occurs. The notifyFxn must implement the following signature: status = notifyFxn(eventType, eventArg, clientArg);

Where: eventType identifies the event being signaled, eventArg is an optional event-specific argument, and clientArg is an arbitrary argument specified by the client at registration. Note that multiple types of events can be specified when registering the notification callback function, but when the callback function is actually called by Power, only a single eventType will be specified for the callback (i.e., the current event). The status returned by the client notification function must be one of the following constants: Power_NOTIFYDONE if the client processed the notification successfully, or Power_NOTIFYERROR if an error occurred during notification.

The clientArg parameter is an arbitrary, client-defined argument to be passed back to the client upon notification. This argument may allow one notify function to be used by multiple instances of a driver (that is, the clientArg can be used to identify the instance of the driver that is being notified).

Parameters
[in]pNotifyObjPower_NotifyObj preallocated by caller
[in]eventTypesevent type or types
[in]notifyFxnclient's Power_NotifyFxn function
[in]clientArgclient-specified argument to pass with notification
Return values
Power_SOKon success.
Power_EINVALIDPOINTERif either pNotifyObj or notifyFxn are NULL.
See also
Power_unregisterNotify()
Using power notify

§ Power_releaseConstraint()

int_fast16_t Power_releaseConstraint ( uint_fast16_t  constraintId)

Release a previously declared constraint.

This function releases a constraint that was previously declared with Power_setConstraint(). For example, if a device driver is starting an I/O transaction and wants to prohibit activation of a sleep state during the transaction, it uses Power_setConstraint() to declare the constraint, before starting the transaction. When the transaction completes, the driver calls this function to release the constraint, to allow the Power manager to once again allow transitions to sleep.

Constraint identifiers are device specific, and defined in the device-specific Power include file. For example, the constraints for MSP432 are defined in PowerMSP432.h.

Only one constraint can be specified with each call to this function; to release multiple constraints this function must be called multiple times.

It is critical that clients call Power_releaseConstraint() when operational constraints no longer exists. Otherwise, Power may be left unnecessarily restricted from activating power savings.

Precondition
Power_setConstraint() must have been called first.
Parameters
[in]constraintIdconstraint id
Returns
CC26XX/CC13XX only: Power_SOK. To minimize code size asserts are used internally to check that the constraintId is valid,valid, and that the constraint count is not already zero; the function always returns Power_SOK.
All other devices: Power_SOK on success, Power_EINVALIDINPUT if the constraintId is invalid, and Power_EFAIL if the constraint count is already zero.
See also
Power_setConstraint()
Using power constraints

§ Power_releaseDependency()

int_fast16_t Power_releaseDependency ( uint_fast16_t  resourceId)

Release a previously declared dependency.

This function releases a dependency that had been previously declared upon a resource (by a call to Power_setDependency()).

Resource identifiers are device specific, and defined in the device-specific Power include file. For example, the resources for CC32XX are defined in PowerCC32XX.h.

Parameters
[in]resourceIdresource id
Returns
CC26XX/CC13XX only: Power_SOK. To minimize code size asserts are used internally to check that the resourceId is valid, and that the resource reference count is not already zero; the function always returns Power_SOK.
All other devices: Power_SOK on success, Power_EINVALIDINPUT if the resourceId is invalid, and Power_EFAIL if the resource reference count is already zero.
See also
Power_setDependency()
Using power dependency

§ Power_reset()

void Power_reset ( void  )

Resets the system and causes it to reboot.

This function causes the system to reset and then boot up again. The impact this has on the existing system state such as what memory is retained is device-specific. Unless otherwise specified in the device-specific documentation, this function will trigger the most comprehensive reset of the system triggerable from software.

§ Power_setConstraint()

int_fast16_t Power_setConstraint ( uint_fast16_t  constraintId)

Declare an operational constraint.

Before taking certain actions, the Power Manager checks to see if the requested action would conflict with a client-declared constraint. If the action does conflict, Power will not proceed with the request. This is the function that allows clients to declare their constraints with Power.

Constraint identifiers are device specific, and defined in the device-specific Power include file. For example, the constraints for MSP432 are defined in PowerMSP432.h.

Only one constraint can be specified with each call to this function; to declare multiple constraints this function must be called multiple times.

Parameters
[in]constraintIdconstraint id
Returns
CC26XX/CC13XX only: Power_SOK. To minimize code size an assert is used internally to check that the constraintId is valid; the function always returns Power_SOK.
All other devices: Power_SOK on success, Power_EINVALIDINPUT if the constraintId is invalid.
See also
Power_releaseConstraint()
Using power constraints

§ Power_setDependency()

int_fast16_t Power_setDependency ( uint_fast16_t  resourceId)

Declare a dependency upon a resource.

This function declares a dependency upon a resource. For example, if a UART driver needs a specific UART peripheral, it uses this function to declare this to the Power Manager. If the resource had been inactive, then Power will activate the peripheral during this function call.

What is needed to make a peripheral resource 'active' will vary by device family. For some devices this may be a simple enable of a clock to the specified peripheral. For others it may also require a power on of a power domain. In either case, the Power Manager will take care of these details, and will also implement reference counting for resources and their interdependencies. For example, if multiple UART peripherals reside in a shared serial power domain, the Power Manager will power up the serial domain when it is first needed, and then automatically power the domain off later, when all related dependencies for the relevant peripherals are released.

Resource identifiers are device specific, and defined in the device-specific Power include file. For example, the resources for CC32XX are defined in PowerCC32XX.h.

Parameters
[in]resourceIdresource id
Returns
CC26XX/CC13XX only: Power_SOK. To minimize code size an assert is used internally to check that the resourceId is valid; the function always returns Power_SOK.
All other devices: Power_SOK on success, Power_EINVALIDINPUT if the reseourceId is invalid.
See also
Power_releaseDependency()
Using power dependency

§ Power_setPerformanceLevel()

int_fast16_t Power_setPerformanceLevel ( uint_fast16_t  level)

Set the MCU performance level.

This function manages a transition to a new device performance level. Before the actual transition is initiated, notifications will be sent to any clients who've registered with Power_registerNotify() for a 'start change performance level' notification. The event name is device specific, and defined in the device-specific Power include file. For example, for MSP432, the event is "PowerMSP432_START_CHANGE_PERF_LEVEL", which is defined in PowerMSP432.h. Once notifications have been completed, the change to the performance level is initiated. After the level change is completed, there is a comparable event that can be used to signal a client that the change has completed. For example, on MSP432 the "PowerMSP432_DONE_CHANGE_PERF_LEVEL" event can be used to signal completion.

This function will not return until the new performance level is in effect. If performance scaling is not supported for the device, or is prohibited by an active constraint, or if the specified level is invalid, then an error status will be returned.

Parameters
[in]levelthe new performance level
Return values
Power_SOKon success.
Power_EINVALIDINPUTif the specified performance level is out of range of valid levels.
Power_EBUSYif another transition is already in progress, or if a single constraint is set to prohibit any change to the performance level.
Power_ECHANGE_NOT_ALLOWEDif a level-specific constraint prohibits a change to the requested level.
Power_EFAILif performance scaling is not supported, if an error occurred during initialization, or if an error occurred during client notifications.
See also
Power_getPerformanceLevel()

§ Power_setPolicy()

void Power_setPolicy ( Power_PolicyFxn  policy)

Set a new Power policy.

This function allows a new Power_PolicyFxn function to be selected at runtime.

Parameters
[in]policythe new Power_PolicyFxn function

§ Power_shutdown()

int_fast16_t Power_shutdown ( uint_fast16_t  shutdownState,
uint_fast32_t  shutdownTime 
)

Put the device into a shutdown state.

This function will transition the device into a shutdown state. Before the actual transition is initiated, notifications will be sent to any clients who've registered (with Power_registerNotify()) for an 'entering shutdown' event. The event name is device specific, and defined in the device-specific Power include file. For example, for CC32XX, the event is "PowerCC32XX_ENTERING_SHUTDOWN", which is defined in PowerCC32XX.h. Once notifications have been completed, the device shutdown will commence.

If the device is successfully transitioned to shutdown, this function call will never return. Upon wakeup, the device and application will be rebooted (through a device reset). If the transition is not successful, one of the error codes listed below will be returned.

On some devices a timed wakeup from shutdown can be specified, using the shutdownTime parameter. This enables an autonomous application reboot at a future time. For example, an application can go to shutdown, and then automatically reboot at a future time to do some work. And once that work is done, the application can shutdown again, for another timed interval. The time interval is specified via the shutdownTime parameter. (On devices that do not support this feature, any value specified for shutdownTime will be ignored.) If the specified shutdownTime is zero, or otherwise less than the total shutdown latency for the device, the shutdownTime parameter will be ignored. The shutdown latency for the device can be found in the device-specific Power include file. For example, for the CC32XX, this latency is defined in PowerCC32XX.h, as "PowerCC32XX_TOTALTIMESHUTDOWN".)

Parameters
[in]shutdownStatethe device-specific shutdown state
[in]shutdownTimethe amount of time (in milliseconds) to keep the the device in the shutdown state; this parameter is not supported on all device families.
Return values
Power_ECHANGE_NOT_ALLOWEDif a constraint is prohibiting shutdown.
Power_EFAILif an error occurred during client notifications.
Power_EINVALIDINPUTif the shutdownState is invalid.
Power_EBUSYif another transition is already in progress.

§ Power_sleep()

int_fast16_t Power_sleep ( uint_fast16_t  sleepState)

Transition the device into a sleep state.

This function is called from the power policy when it has made a decision to put the device in a specific sleep state. This function returns to the caller (the policy function) once the device has awoken from sleep.

Warning
This function must be called with interrupts disabled, and should not be called directly by the application, or by any drivers. This function does not check declared constraints; the policy function must check constraints before calling this function to initiate sleep.
Parameters
[in]sleepStatethe sleep state
Return values
Power_SOKon success, the device has slept and is awake again.
Power_EFAILif an error occurred during client notifications, or if a general failure occurred.
Power_EINVALIDINPUTif the sleepState is invalid.
Power_EBUSYif another transition is already in progress.

§ Power_unregisterNotify()

void Power_unregisterNotify ( Power_NotifyObj pNotifyObj)

Unregister previously registered notifications.

This function unregisters for event notifications that were previously registered with Power_registerNotify(). The caller must specify a pointer to the same notification object used during registration.

Parameters
[in]pNotifyObjThe Power_NotifyObj used with the original call to Power_registerNotify()
See also
Power_registerNotify()
Using power notify
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale