Modules | |
Status Codes | |
Command Codes | |
Macros | |
#define | SD_CMD_RESERVED (32) |
#define | SD_STATUS_RESERVED (-32) |
#define SD_CMD_RESERVED (32) |
Common SD_control() command code reservation offset. SD driver implementations should offset command codes with SD_CMD_RESERVED growing positively.
Example implementation specific command codes:
#define SD_STATUS_RESERVED (-32) |
Common SD_control status code reservation offset. SD driver implementations should offset status codes with SD_STATUS_RESERVED growing negatively.
Example implementation specific status codes: