rflib
|
#include <RFCC26X2.h>
Data Fields | |
uint32_t | startTime |
Start time in RAT Ticks for the radio command. More... | |
RF_StartType | startType |
Start type for the start time. More... | |
uint32_t | allowDelay |
uint32_t | endTime |
End time in RAT Ticks for the radio command. More... | |
RF_EndType | endType |
End type for the end time. More... | |
uint32_t | duration |
Duration in RAT Ticks for the radio command. More... | |
uint32_t | activityInfo |
Activity info provided by user. More... | |
RF_PriorityCoex | coexPriority |
Priority to use for coexistence request. More... | |
RF_RequestCoex | coexRequest |
REQUEST line behavior to use for coexistence request. More... | |
uint32_t RF_ScheduleCmdParams::startTime |
Start time in RAT Ticks for the radio command.
RF_StartType RF_ScheduleCmdParams::startType |
Start type for the start time.
uint32_t RF_ScheduleCmdParams::allowDelay |
Control word to define the policy of the scheduler if the timing of a command cannot be met. Only applicable on CC13x2 and CC26x2 devices. RF_AllowDelayNone: Reject the command. RF_AllowDelayAny: Append the command to the end of the queue.
uint32_t RF_ScheduleCmdParams::endTime |
End time in RAT Ticks for the radio command.
RF_EndType RF_ScheduleCmdParams::endType |
End type for the end time.
uint32_t RF_ScheduleCmdParams::duration |
Duration in RAT Ticks for the radio command.
uint32_t RF_ScheduleCmdParams::activityInfo |
Activity info provided by user.
RF_PriorityCoex RF_ScheduleCmdParams::coexPriority |
Priority to use for coexistence request.
RF_RequestCoex RF_ScheduleCmdParams::coexRequest |
REQUEST line behavior to use for coexistence request.