Z-Stack API Reference  7.10.00.10
_zstack_sysOtaMsg_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t cmd
 
uint8_t * pData
 pointer to App Data
 

Detailed Description

Structure to return the system OTA message.

Field Documentation

§ cmd

uint8_t cmd

Command


The documentation for this struct was generated from the following file: