Z-Stack API Reference  7.10.00.10
_zstack_zdotcteviceind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t nwkAddr
 
uint16_t parentAddr
 
zstack_LongAddr_t extendedAddr
 

Detailed Description

Structure to send a ZDO Trust Center Device Indication.

Field Documentation

§ extendedAddr

zstack_LongAddr_t extendedAddr

The joining device's 64-bit extended address

§ nwkAddr

uint16_t nwkAddr

The joining device's network address

§ parentAddr

uint16_t parentAddr

The joining device's parent's network address


The documentation for this struct was generated from the following file: