Z-Stack API Reference  7.10.00.10
zclDoorLockGetYearDayScheduleRsp_t Struct Reference

Client Commands Received: Get Year Day Schedule Response. More...

#include <zcl_closures.h>

Data Fields

uint8_t scheduleID
 number is between 0 - [# of Week Day Schedules Per User attribute].
 
uint16_t userID
 is between 0 - [# of Total Users Supported attribute].
 
uint8_t status
 Request status.
 
uint32_t zigBeeLocalStartTime
 Start time and end time are given in LocalTime.
 
uint32_t zigBeeLocalEndTime
 End of Holiday time.
 

Detailed Description

Client Commands Received: Get Year Day Schedule Response.


The documentation for this struct was generated from the following file: