Z-Stack API Reference  7.10.00.10
zclGpTableResponse_t Struct Reference

Data Fields

uint8_t status
 Response status.
 
uint8_t tableEntriesTotal
 Total number of entries.
 
uint8_t startIndex
 Index of the first entry on the response.
 
uint8_t entriesCount
 Number of entries in the response.
 
uint8_t * entry
 List of entries.
 

The documentation for this struct was generated from the following file: