71 #ifndef ti_drivers_aesgcm_AESGCMCC26XX__include 72 #define ti_drivers_aesgcm_AESGCMCC26XX__include AESGCM_CallbackFxn callbackFxn
Definition: AESGCMCC26XX.h:127
The CryptoKey type is an opaque representation of a cryptographic key.
AESGCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESGCM.h:868
bool operationCanceled
Definition: AESGCMCC26XX.h:122
AESGCM_Operation * operation
Definition: AESGCMCC26XX.h:128
Semaphore module for the RTOS Porting Interface.
uint32_t semaphoreTimeout
Definition: AESGCMCC26XX.h:126
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: AESGCMCC26XX.h:110
void(* AESGCM_CallbackFxn)(AESGCM_Handle handle, int_fast16_t returnValue, AESGCM_OperationUnion *operation, AESGCM_OperationType operationType)
The definition of a callback function used by the AESGCM driver when used in AESGCM_RETURN_BEHAVIOR_C...
Definition: AESGCM.h:898
AESGCM_ReturnBehavior
The way in which GCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESGCM.h:682
Software Interrupt module for the RTOS Porting Interface.
AESGCM_OperationType operationType
Definition: AESGCMCC26XX.h:125
bool operationInProgress
Definition: AESGCMCC26XX.h:121
AESGCMCC26XX Hardware Attributes.
Definition: AESGCMCC26XX.h:95
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a me...
Definition: AESGCM.h:716
bool isOpen
Definition: AESGCMCC26XX.h:120
int_fast16_t returnStatus
Definition: AESGCMCC26XX.h:123
AESGCMCC26XX Object.
Definition: AESGCMCC26XX.h:118
Hardware Interrupt module for the RTOS Porting Interface.
AESGCM_ReturnBehavior returnBehavior
Definition: AESGCMCC26XX.h:124