![]() |
![]() |
Attestation driver header.
============================================================================
This file contains the APIs to generate an attestation token and obtain the expected token size to create a buffer to store the generated token. Attestation_PSA APIs are only available when TF-M is enabled and this file provides the non-secure interface to the Attestation_PSA driver.
After calling the Attestation initialization function, a token can be generated using the challenge provided by the attestation service to Attestation_PSA API. To generate a token, Attestation_PSA APIs assume that attestation keys are pre-provisioned in the pre-provisioned key sector.
#include <stdint.h>#include <stddef.h>#include <psa/initial_attestation.h>
Go to the source code of this file.
Macros | |
| #define | ATTESTATION_PSA_MAX_TOKEN_SIZE (PSA_INITIAL_ATTEST_MAX_TOKEN_SIZE) |
| Maximum attestation token size. More... | |
| #define | ATTESTATION_PSA_STATUS_SUCCESS ((int_fast16_t)0) |
| Successful status code. More... | |
| #define | ATTESTATION_PSA_STATUS_ERROR ((int_fast16_t)-1) |
| Generic error status code. More... | |
| #define | ATTESTATION_PSA_STATUS_RESOURCE_UNAVAILABLE ((int_fast16_t)-2) |
| An error status code returned if the hardware or software resource is currently unavailable. More... | |
| #define | ATTESTATION_PSA_STATUS_INVALID_INPUTS ((int_fast16_t)-3) |
| Operation failed due to invalid inputs. More... | |
Functions | |
| int_fast16_t | Attestation_PSA_getToken (const uint8_t *auth_challenge, size_t challenge_size, uint8_t *token_buf, size_t token_buf_size, size_t *token_size) |
| Get initial attestation token. More... | |
| int_fast16_t | Attestation_PSA_getTokenSize (size_t challenge_size, size_t *token_size) |
| Get the exact size of initial attestation token in bytes. More... | |
| void | Attestation_PSA_init (void) |
| This function initializes the Attestation module. More... | |
| #define ATTESTATION_PSA_MAX_TOKEN_SIZE (PSA_INITIAL_ATTEST_MAX_TOKEN_SIZE) |
Maximum attestation token size.
The maximum size of an attestation token that can be generated by the attestation service. Used to configure buffers for services that verify the produced tokens.
| #define ATTESTATION_PSA_STATUS_SUCCESS ((int_fast16_t)0) |
Successful status code.
Functions return ATTESTATION_PSA_STATUS_SUCCESS if the function was executed successfully.
| #define ATTESTATION_PSA_STATUS_ERROR ((int_fast16_t)-1) |
Generic error status code.
Functions return ATTESTATION_PSA_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.
| #define ATTESTATION_PSA_STATUS_RESOURCE_UNAVAILABLE ((int_fast16_t)-2) |
An error status code returned if the hardware or software resource is currently unavailable.
Attestation driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.
| #define ATTESTATION_PSA_STATUS_INVALID_INPUTS ((int_fast16_t)-3) |
Operation failed due to invalid inputs.
Functions return ATTESTATION_PSA_STATUS_INVALID_INPUTS if input validation fails.
| int_fast16_t Attestation_PSA_getToken | ( | const uint8_t * | auth_challenge, |
| size_t | challenge_size, | ||
| uint8_t * | token_buf, | ||
| size_t | token_buf_size, | ||
| size_t * | token_size | ||
| ) |
Get initial attestation token.
| [in] | auth_challenge | Pointer to buffer where challenge input is stored. |
| [in] | challenge_size | Size of challenge object in bytes. Must be 32, 48, or 64-bytes. |
| [out] | token_buf | Pointer to the buffer where attestation token will be stored, with a maximum buffer size of ATTESTATION_PSA_MAX_TOKEN_SIZE. |
| [in] | token_buf_size | Size of allocated buffer for token, in bytes. |
| [out] | token_size | Size of the token that has been returned, in bytes. |
| ATTESTATION_PSA_STATUS_SUCCESS | The operation succeeded. |
| ATTESTATION_PSA_STATUS_ERROR | The operation failed. |
| ATTESTATION_PSA_STATUS_RESOURCE_UNAVAILABLE | The required hardware resource was not available. Try again later. |
| ATTESTATION_PSA_STATUS_INVALID_INPUTS | Input validation failed. |
| int_fast16_t Attestation_PSA_getTokenSize | ( | size_t | challenge_size, |
| size_t * | token_size | ||
| ) |
Get the exact size of initial attestation token in bytes.
Returns the size of the IAT token. It can be used if the caller dynamically allocates memory for the token buffer.
| [in] | challenge_size | Size of challenge object in bytes. Must be 32, 48, or 64-bytes. |
| [out] | token_size | Size of the token in bytes, which is created by initial attestation service. |
| ATTESTATION_PSA_STATUS_SUCCESS | The operation succeeded. |
| ATTESTATION_PSA_STATUS_ERROR | The operation failed. |
| ATTESTATION_PSA_STATUS_RESOURCE_UNAVAILABLE | The required hardware resource was not available. Try again later. |
| ATTESTATION_PSA_STATUS_INVALID_INPUTS | Input validation failed. |
| void Attestation_PSA_init | ( | void | ) |
This function initializes the Attestation module.