45 #ifndef ti_drivers_timer_TimerCC26XX__include 46 #define ti_drivers_timer_TimerCC26XX__include TimerCC26XX_Object.
Definition: TimerCC26XX.h:119
GPTimer driver implementation for CC26XX/CC13XX.
Definition: TimerCC26XX.h:72
TimerCC26XX_SubTimer subTimer
Definition: TimerCC26XX.h:110
TimerCC26XX_SubTimer
Definition: TimerCC26XX.h:70
Semaphore module for the RTOS Porting Interface.
TIMER_BASE_OBJECT GPTimerCC26XX_Handle gptHandle
Definition: TimerCC26XX.h:124
bool isOpen
Definition: TimerCC26XX.h:127
TimerCC26XX Hardware Attributes.
Definition: TimerCC26XX.h:102
TIMER_BASE_HWATTRS uint8_t gpTimerUnit
Definition: TimerCC26XX.h:107
Definition: TimerCC26XX.h:73
Definition: TimerCC26XX.h:74
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:404