A structure containing the parameters of an elliptic curve. More...
#include <ECCParams.h>
Data Fields | |
const ECCParams_CurveType | curveType |
const uint8_t * | prime |
const uint8_t * | a |
const uint8_t * | b |
const uint8_t * | order |
const uint8_t | cofactor |
const size_t | length |
const uint8_t * | generatorX |
const uint8_t * | generatorY |
A structure containing the parameters of an elliptic curve.
Elliptical Curve Cryptography (ECC) prime curve parameters.
const ECCParams_CurveType ECCParams_CurveParams::curveType |
const uint8_t* ECCParams_CurveParams::prime |
const uint8_t* ECCParams_CurveParams::a |
const uint8_t* ECCParams_CurveParams::b |
const uint8_t* ECCParams_CurveParams::order |
const uint8_t ECCParams_CurveParams::cofactor |
const size_t ECCParams_CurveParams::length |
const uint8_t* ECCParams_CurveParams::generatorX |
const uint8_t* ECCParams_CurveParams::generatorY |