LogSinkUART Sink parameters. More...
#include <LogSinkUART.h>
Data Fields | |
uint_least8_t | index |
LogSinkUART Sink parameters.
The LogSinkUART_Instance structure contains a set of parameters used to characterize a LogSinkUART sink.
uint_least8_t LogSinkUART_Instance::index |
Index of the LogSinkUART sink instance used to index LogSinkUART_config
[]