Data Structures | Macros | Typedefs | Functions | Variables
CryptoKey.h File Reference

Detailed Description

The CryptoKey type is an opaque representation of a cryptographic key.

============================================================================

Warning
This is a beta API. It may change in future releases.

Cryptographic keying material may be stored on an embedded system multiple ways.

Each storage option requires different approaches to handling the keying material when performing a crypto operation. In order to separate these concerns from the API of the various crypto drivers available with TI-RTOS, the CryptoKey type abstracts away from these details. It does not contain any cryptographic keying material itself but instead contains the details necessary for drivers to use the keying material. The driver implementation handles preparing and moving the keying material as necessary to perform the desired crypto operation.

The same CryptoKey may be passed to crypto APIs of different modes subject to restrictions placed on the key by their storage types. Plaintext keys may be used without restriction while key store keys have their permitted uses restricted when the keying material is loaded. These restrictions are specified in a CryptoKey_SecurityPolicy that is device-specific and depends on the hardware capability of the device.

An application should never access a field within a CryptoKey struct itself. Where needed, helper functions are provided to do so.

Before using a CryptoKey in another crypto API call, it must be initialized with a call to one of the initialization functions.

The keystore CryptoKeys may be used to load a key into a key store after its respective _init call.

CryptoKeys can be initialized "blank", without keying material but with an empty buffer or key store entry, to encode the destination of a key to be created in the future. This way, keys may be generated securely within a key store for example and never even be stored in RAM temporarily.

Not all devices support all CryptoKey functionality. This is hardware-dependent.

#include <stdint.h>
#include <stdbool.h>
Include dependency graph for CryptoKey.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  CryptoKey_Plaintext
 Plaintext CryptoKey datastructure. More...
 
struct  CryptoKey_KeyStore
 Key store CryptoKey datastructure. More...
 
struct  CryptoKey
 CryptoKey datastructure. More...
 

Macros

#define CryptoKey_STATUS_RESERVED   (-32)
 
#define CryptoKey_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define CryptoKey_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define CryptoKey_STATUS_UNDEFINED_ENCODING   (-2)
 Returned if the encoding of a CryptoKey is not a CryptoKey_Encoding value. More...
 
#define CRYPTOKEY_HSM   0x20U
 
#define CRYPTOKEY_PLAINTEXT   0x02U
 
#define CRYPTOKEY_BLANK_PLAINTEXT   0x04U
 
#define CRYPTOKEY_KEYSTORE   0x08U
 
#define CRYPTOKEY_BLANK_KEYSTORE   0x10U
 

Typedefs

typedef uint8_t CryptoKey_Encoding
 List of the different types of CryptoKey. _HSM encodings are only available for select devices, CC27XX. More...
 
typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy
 Structure that specifies the restrictions on a CryptoKey. More...
 

Functions

int_fast16_t CryptoKey_getCryptoKeyType (const CryptoKey *keyHandle, CryptoKey_Encoding *keyType)
 Gets the key type of the CryptoKey. More...
 
int_fast16_t CryptoKey_isBlank (const CryptoKey *keyHandle, bool *isBlank)
 Whether the CryptoKey is 'blank' or represents valid keying material. More...
 
int_fast16_t CryptoKey_initSecurityPolicy (CryptoKey_SecurityPolicy *policy)
 Function to initialize the CryptoKey_SecurityPolicy struct to its defaults. More...
 
int_fast16_t CryptoKey_verifySecureInputKey (const CryptoKey *secureKey)
 Function to verify a secure CryptoKey. More...
 
int_fast16_t CryptoKey_verifySecureOutputKey (const CryptoKey *secureKey)
 Function to verify a secure output CryptoKey. More...
 
int_fast16_t CryptoKey_copySecureInputKey (CryptoKey *dst, const CryptoKey **src)
 Function to copy and verify a secure input CryptoKey. More...
 
int_fast16_t CryptoKey_copySecureOutputKey (CryptoKey *dst, CryptoKey **src)
 Function to copy and verify a secure output CryptoKey. More...
 

Variables

static const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U
 
static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U
 
static const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U
 
static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U
 
static const CryptoKey_Encoding CryptoKey_PLAINTEXT_HSM = 0x02U | 0x20U
 
static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT_HSM = 0x04U | 0x20U
 
static const CryptoKey_Encoding CryptoKey_KEYSTORE_HSM = 0x08U | 0x20U
 
static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE_HSM = 0x10U | 0x20U
 

Macro Definition Documentation

§ CRYPTOKEY_HSM

#define CRYPTOKEY_HSM   0x20U

§ CRYPTOKEY_PLAINTEXT

#define CRYPTOKEY_PLAINTEXT   0x02U

§ CRYPTOKEY_BLANK_PLAINTEXT

#define CRYPTOKEY_BLANK_PLAINTEXT   0x04U

§ CRYPTOKEY_KEYSTORE

#define CRYPTOKEY_KEYSTORE   0x08U

§ CRYPTOKEY_BLANK_KEYSTORE

#define CRYPTOKEY_BLANK_KEYSTORE   0x10U

Typedef Documentation

§ CryptoKey_Encoding

typedef uint8_t CryptoKey_Encoding

List of the different types of CryptoKey. _HSM encodings are only available for select devices, CC27XX.

§ CryptoKey_SecurityPolicy

typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy

Structure that specifies the restrictions on a CryptoKey.

This structure is device-specific and declared here in incomplete form. The structure is fully defined in CryptoKeyDEVICE.h. This creates a link-time binding when using the structure with key store functions. If the instance of the CryptoKey_SecurityPolicy is kept in a device-specific application-file, the generic application code may still use references to it despite being an incomplete type in the generic application file at compile time.

Function Documentation

§ CryptoKey_getCryptoKeyType()

int_fast16_t CryptoKey_getCryptoKeyType ( const CryptoKey keyHandle,
CryptoKey_Encoding keyType 
)

Gets the key type of the CryptoKey.

Parameters
[in]keyHandlePointer to a CryptoKey
[out]keyTypeType of the CryptoKey
Returns
Returns a status code

§ CryptoKey_isBlank()

int_fast16_t CryptoKey_isBlank ( const CryptoKey keyHandle,
bool *  isBlank 
)

Whether the CryptoKey is 'blank' or represents valid keying material.

Parameters
[in]keyHandlePointer to a CryptoKey
[out]isBlankWhether the CryptoKey is 'blank' or not
Returns
Returns a status code

§ CryptoKey_initSecurityPolicy()

int_fast16_t CryptoKey_initSecurityPolicy ( CryptoKey_SecurityPolicy policy)

Function to initialize the CryptoKey_SecurityPolicy struct to its defaults.

This will zero-out all fields that cannot be set to safe defaults

Parameters
[in]policyPointer to a CryptoKey_SecurityPolicy
Returns
Returns a status code

§ CryptoKey_verifySecureInputKey()

int_fast16_t CryptoKey_verifySecureInputKey ( const CryptoKey secureKey)

Function to verify a secure CryptoKey.

This will check that the key type is valid and verify plaintext key material is located in non-secure read-access memory.

Note
This function may not be available in all implementations
Parameters
[in]secureKeyPointer to a CryptoKey struct located in secure memory
Return values
CryptoKey_STATUS_SUCCESSKey passes all verification checks
CryptoKey_STATUS_ERRORKey fails any verification check

§ CryptoKey_verifySecureOutputKey()

int_fast16_t CryptoKey_verifySecureOutputKey ( const CryptoKey secureKey)

Function to verify a secure output CryptoKey.

This will check that the key type is valid and verify plaintext key material is located in non-secure RW-access memory.

Note
This function may not be available in all implementations
Parameters
[in]secureKeyPointer to a CryptoKey struct located in secure memory
Return values
CryptoKey_STATUS_SUCCESSKey passes all verification checks
CryptoKey_STATUS_ERRORKey fails any verification check

§ CryptoKey_copySecureInputKey()

int_fast16_t CryptoKey_copySecureInputKey ( CryptoKey dst,
const CryptoKey **  src 
)

Function to copy and verify a secure input CryptoKey.

This will check that the source CryptoKey struct is located in non-secure read-access memory, copy the CryptoKey struct from the src to dst, and check that the key type is valid and verify plaintext key material is located in non-secure read-access memory.

Note
This function may not be available in all implementations
Parameters
[out]dstPointer to the destination CryptoKey struct located in secure memory
[in,out]srcPointer to a source CryptoKey struct pointer located in secure memory which will be updated to point to the destination CryptoKey struct
Return values
CryptoKey_STATUS_SUCCESSKey passes all verification checks
CryptoKey_STATUS_ERRORKey fails any verification check

§ CryptoKey_copySecureOutputKey()

int_fast16_t CryptoKey_copySecureOutputKey ( CryptoKey dst,
CryptoKey **  src 
)

Function to copy and verify a secure output CryptoKey.

This will check that the source CryptoKey struct is located in non-secure RW-access memory, copy the CryptoKey struct from the src to dst, and check that the key type is valid and verify plaintext key material is located in non-secure RW-access memory.

Note
This function may not be available in all implementations
Parameters
[out]dstPointer to the destination CryptoKey struct located in secure memory
[in,out]srcPointer to a source CryptoKey struct pointer located in secure memory which will be updated to point to the destination CryptoKey struct
Return values
CryptoKey_STATUS_SUCCESSKey passes all verification checks
CryptoKey_STATUS_ERRORKey fails any verification check

Variable Documentation

§ CryptoKey_PLAINTEXT

const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U
static

§ CryptoKey_BLANK_PLAINTEXT

const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U
static

§ CryptoKey_KEYSTORE

const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U
static

§ CryptoKey_BLANK_KEYSTORE

const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U
static

§ CryptoKey_PLAINTEXT_HSM

const CryptoKey_Encoding CryptoKey_PLAINTEXT_HSM = 0x02U | 0x20U
static

§ CryptoKey_BLANK_PLAINTEXT_HSM

const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT_HSM = 0x04U | 0x20U
static

§ CryptoKey_KEYSTORE_HSM

const CryptoKey_Encoding CryptoKey_KEYSTORE_HSM = 0x08U | 0x20U
static

§ CryptoKey_BLANK_KEYSTORE_HSM

const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE_HSM = 0x10U | 0x20U
static
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale