Z-Stack API Reference  8.30.00.09
gpTableReqCmd_t Struct Reference

Data Fields

uint8_t options
 Options for table request.
 
uint32_t gpdId
 ID of the GPD.
 
uint8_t gpdIEEE [Z_EXTADDR_LEN]
 0b010. More...
 
uint8_t ep
 is 0b010. More...
 
uint8_t index
 requested. More...
 

Field Documentation

§ ep

uint8_t ep

is 0b010.

Endpoint of the GP if application ID

§ gpdIEEE

uint8_t gpdIEEE[Z_EXTADDR_LEN]

0b010.

IEEE of the GPD if application ID is

§ index

uint8_t index

requested.

index value of the Proxy Table entry being


The documentation for this struct was generated from the following file: