Data Fields
AESGCM_s_SecureCallback Struct Reference

#include <AESGCMCC26X4_s.h>

Collaboration diagram for AESGCM_s_SecureCallback:
Collaboration graph
[legend]

Data Fields

SecureCallback_Object object
 
AESGCM_Handle handle
 
int_fast16_t returnValue
 
AESGCM_OperationUnionoperation
 
AESGCM_OperationType operationType
 

Field Documentation

§ object

SecureCallback_Object AESGCM_s_SecureCallback::object

§ handle

AESGCM_Handle AESGCM_s_SecureCallback::handle

§ returnValue

int_fast16_t AESGCM_s_SecureCallback::returnValue

§ operation

AESGCM_OperationUnion* AESGCM_s_SecureCallback::operation

§ operationType

AESGCM_OperationType AESGCM_s_SecureCallback::operationType

The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale