|  |  | 
| rflib
    | 
#include "rf_mailbox.h"
Go to the source code of this file.
| Macros | |
| Operation not finished | |
| #define | IEEE_SUSPENDED 0x2001 | 
| Operation suspended.  More... | |
| Operation finished normally | |
| #define | IEEE_DONE_OK 0x2400 | 
| Operation ended normally.  More... | |
| #define | IEEE_DONE_BUSY 0x2401 | 
| CSMA-CA operation ended with failure.  More... | |
| #define | IEEE_DONE_STOPPED 0x2402 | 
| Operation stopped after stop command.  More... | |
| #define | IEEE_DONE_ACK 0x2403 | 
| ACK packet received with pending data bit cleared.  More... | |
| #define | IEEE_DONE_ACKPEND 0x2404 | 
| ACK packet received with pending data bit set.  More... | |
| #define | IEEE_DONE_TIMEOUT 0x2405 | 
| Operation ended due to timeout.  More... | |
| #define | IEEE_DONE_BGEND 0x2406 | 
| operation ended  More... | |
| #define | IEEE_DONE_ABORT 0x2407 | 
| Operation aborted by command.  More... | |
| Operation finished with error | |
| #define | IEEE_ERROR_PAR 0x2800 | 
| Illegal parameter.  More... | |
| #define | IEEE_ERROR_NO_SETUP 0x2801 | 
| Operation using Rx or Tx attempted when not in 15.4 mode.  More... | |
| #define | IEEE_ERROR_NO_FS 0x2802 | 
| Operation using Rx or Tx attempted without frequency synth configured.  More... | |
| #define | IEEE_ERROR_SYNTH_PROG 0x2803 | 
| Synthesizer programming failed to complete on time.  More... | |
| #define | IEEE_ERROR_RXOVF 0x2804 | 
| Receiver overflowed during operation.  More... | |
| #define | IEEE_ERROR_TXUNF 0x2805 | 
| Transmitter underflowed during operation.  More... | |
| #define IEEE_SUSPENDED 0x2001 | 
Operation suspended.
| #define IEEE_DONE_OK 0x2400 | 
Operation ended normally.
| #define IEEE_DONE_BUSY 0x2401 | 
CSMA-CA operation ended with failure.
| #define IEEE_DONE_STOPPED 0x2402 | 
Operation stopped after stop command.
| #define IEEE_DONE_ACK 0x2403 | 
ACK packet received with pending data bit cleared.
| #define IEEE_DONE_ACKPEND 0x2404 | 
ACK packet received with pending data bit set.
| #define IEEE_DONE_TIMEOUT 0x2405 | 
Operation ended due to timeout.
| #define IEEE_DONE_BGEND 0x2406 | 
operation ended
FG operation ended because necessary background level
| #define IEEE_DONE_ABORT 0x2407 | 
Operation aborted by command.
| #define IEEE_ERROR_PAR 0x2800 | 
Illegal parameter.
| #define IEEE_ERROR_NO_SETUP 0x2801 | 
Operation using Rx or Tx attempted when not in 15.4 mode.
| #define IEEE_ERROR_NO_FS 0x2802 | 
Operation using Rx or Tx attempted without frequency synth configured.
| #define IEEE_ERROR_SYNTH_PROG 0x2803 | 
Synthesizer programming failed to complete on time.
| #define IEEE_ERROR_RXOVF 0x2804 | 
Receiver overflowed during operation.
| #define IEEE_ERROR_TXUNF 0x2805 | 
Transmitter underflowed during operation.