![]()  | 
  ![]()  | 
| 
    rflib
    
   | 
 
RF_ratCapture parameter structure. More...
#include <RFCC26X2.h>

Data Fields | |
| RF_RatCallback | callback | 
| Callback function to be invoked upon a capture event (optional).  More... | |
| RF_RatHandle | channel | 
| RF_RatHandle identifies the channel to be allocated.  More... | |
| RF_RatCaptureSource | source | 
| Configuration of the event source to cause a capture event.  More... | |
| RF_RatCaptureMode | captureMode | 
| Configuration of the mode of event to cause a capture event.  More... | |
| RF_RatCaptureRepetition | repeat | 
| Configuration of the channel to be used in single or repeated mode.  More... | |
RF_ratCapture parameter structure.
RF_RatCapture parameters are used with the RF_ratCapture() call.
| RF_RatCallback RF_RatConfigCapture::callback | 
Callback function to be invoked upon a capture event (optional).
| RF_RatHandle RF_RatConfigCapture::channel | 
RF_RatHandle identifies the channel to be allocated.
| RF_RatCaptureSource RF_RatConfigCapture::source | 
Configuration of the event source to cause a capture event.
| RF_RatCaptureMode RF_RatConfigCapture::captureMode | 
Configuration of the mode of event to cause a capture event.
| RF_RatCaptureRepetition RF_RatConfigCapture::repeat | 
Configuration of the channel to be used in single or repeated mode.