![]()  | 
  ![]()  | 
| 
    rflib
    
   | 
 
Bluetooth 5 PHY Test Transmitter Command. More...
#include <rf_ble_cmd.h>

Data Fields | |
| uint16_t | commandNo | 
| The command ID number 0x182A.  More... | |
| uint16_t | status | 
| An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.  More... | |
| rfc_radioOp_t * | pNextOp | 
| Pointer to the next operation to run after this operation is done.  More... | |
| ratmr_t | startTime | 
Absolute or relative start time (depending on the value of startTrigger)  More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| uint8_t | channel | 
| Channel to use 0–39: BLE advertising/data channel index 60–207: Custom frequency; (2300 + channel) MHz255: Use existing frequency Others: Reserved More...  | |
| struct { | |
| uint8_t init:7 | |
If bOverride = 1 or custom frequency is used:0: Do not use whitening Other value: Initialization for 7-bit LFSR whitener. More...  | |
| uint8_t bOverride:1 | |
| 0: Use default whitening for BLE advertising/data channels 1: Override whitening initialization with value of init More...  | |
| } | whitening | 
| struct { | |
| uint8_t mainMode:2 | |
| PHY to use: 0: 1 Mbps 1: 2 Mbps 2: Coded 3: Reserved More...  | |
| uint8_t coding:6 | |
| Coding to use for TX if coded PHY is selected. See the Technical Reference Manual for details.  More... | |
| } | phyMode | 
| uint8_t | rangeDelay | 
| Number of RAT ticks to add to the listening time after T_IFS.  More... | |
| uint16_t | txPower | 
| Transmit power to use (overrides the one given in radio setup)  0x0000: Use default TX power 0xFFFF: 20-dBm PA only: Use TX power from tx20Power field (command structure that includes tx20Power must be used)  More... | |
| rfc_bleTxTestPar_t * | pParams | 
| Pointer to command specific parameter structure.  More... | |
| rfc_bleTxTestOutput_t * | pOutput | 
| Pointer to command specific output structure.  More... | |
| uint32_t | tx20Power | 
If txPower = 0xFFFF:If tx20Power < 0x10000000: Transmit power to use for the 20-dBm PA; overrides the one given in radio setup for the duration of the command. If tx20Power >= 0x10000000: Pointer to PA change override structure as for CMD_CHANGE_PA ; permanently changes the PA and PA power set in radio setup.For other values of txPower, this field is not accessed by the radio CPU and may be omitted from the structure.  More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| struct { | |
| uint8_t init:7 | |
If bOverride = 1 or custom frequency is used:0: Do not use whitening Other value: Initialization for 7-bit LFSR whitener. More...  | |
| uint8_t bOverride:1 | |
| 0: Use default whitening for BLE advertising/data channels 1: Override whitening initialization with value of init More...  | |
| } | whitening | 
| struct { | |
| uint8_t mainMode:2 | |
| PHY to use: 0: 1 Mbps 1: 2 Mbps 2: Coded 3: Reserved More...  | |
| uint8_t coding:6 | |
| Coding to use for TX if coded PHY is selected. See the Technical Reference Manual for details.  More... | |
| } | phyMode | 
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| struct { | |
| uint8_t init:7 | |
If bOverride = 1 or custom frequency is used:0: Do not use whitening Other value: Initialization for 7-bit LFSR whitener. More...  | |
| uint8_t bOverride:1 | |
| 0: Use default whitening for BLE advertising/data channels 1: Override whitening initialization with value of init More...  | |
| } | whitening | 
| struct { | |
| uint8_t mainMode:2 | |
| PHY to use: 0: 1 Mbps 1: 2 Mbps 2: Coded 3: Reserved More...  | |
| uint8_t coding:6 | |
| Coding to use for TX if coded PHY is selected. See the Technical Reference Manual for details.  More... | |
| } | phyMode | 
Bluetooth 5 PHY Test Transmitter Command.
| uint16_t rfc_CMD_BLE5_TX_TEST_s::commandNo | 
The command ID number 0x182A.
| uint16_t rfc_CMD_BLE5_TX_TEST_s::status | 
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
| rfc_radioOp_t * rfc_CMD_BLE5_TX_TEST_s::pNextOp | 
Pointer to the next operation to run after this operation is done.
| ratmr_t rfc_CMD_BLE5_TX_TEST_s::startTime | 
Absolute or relative start time (depending on the value of startTrigger) 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::triggerType | 
The type of trigger.
| uint8_t rfc_CMD_BLE5_TX_TEST_s::bEnaCmd | 
0: No alternative trigger command
 1: CMD_TRIGGER can be used as an alternative trigger 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::triggerNo | 
The trigger number of the CMD_TRIGGER command that triggers this action.
| uint8_t rfc_CMD_BLE5_TX_TEST_s::pastTrig | 
0: A trigger in the past is never triggered, or for start of commands, give an error
 1: A trigger in the past is triggered as soon as possible 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::startTrigger | 
Identification of the trigger that starts the operation.
| uint8_t rfc_CMD_BLE5_TX_TEST_s::rule | 
Condition for running next command: Rule for how to proceed.
| uint8_t rfc_CMD_BLE5_TX_TEST_s::nSkip | 
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::condition | 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::channel | 
Channel to use
 0–39: BLE advertising/data channel index
 60–207: Custom frequency; (2300 + channel) MHz
 255: Use existing frequency
 Others: Reserved 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::init | 
If bOverride = 1 or custom frequency is used:
 0: Do not use whitening
 Other value: Initialization for 7-bit LFSR whitener. 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::bOverride | 
0: Use default whitening for BLE advertising/data channels
 1: Override whitening initialization with value of init 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::whitening | 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::mainMode | 
PHY to use:
 0: 1 Mbps
 1: 2 Mbps
 2: Coded
 3: Reserved 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::coding | 
Coding to use for TX if coded PHY is selected. See the Technical Reference Manual for details.
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::phyMode | 
| uint8_t rfc_CMD_BLE5_TX_TEST_s::rangeDelay | 
Number of RAT ticks to add to the listening time after T_IFS.
| uint16_t rfc_CMD_BLE5_TX_TEST_s::txPower | 
Transmit power to use (overrides the one given in radio setup) 
 0x0000: Use default TX power
 0xFFFF: 20-dBm PA only: Use TX power from tx20Power field (command structure that includes tx20Power must be used) 
| rfc_bleTxTestPar_t * rfc_CMD_BLE5_TX_TEST_s::pParams | 
Pointer to command specific parameter structure.
| rfc_bleTxTestOutput_t * rfc_CMD_BLE5_TX_TEST_s::pOutput | 
Pointer to command specific output structure.
| uint32_t rfc_CMD_BLE5_TX_TEST_s::tx20Power | 
If txPower = 0xFFFF:
 If tx20Power < 0x10000000: Transmit power to use for the 20-dBm PA; overrides the one given in radio setup for the duration of the command. 
 If tx20Power >= 0x10000000: Pointer to PA change override structure as for CMD_CHANGE_PA ; permanently changes the PA and PA power set in radio setup.
 For other values of txPower, this field is not accessed by the radio CPU and may be omitted from the structure. 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::startTrigger | 
Identification of the trigger that starts the operation.
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::condition | 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::whitening | 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::phyMode | 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::startTrigger | 
Identification of the trigger that starts the operation.
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::condition | 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::whitening | 
| struct { ... } rfc_CMD_BLE5_TX_TEST_s::phyMode |