![]()  | 
  ![]()  | 
| 
    rflib
    
   | 
 
Flush Data Queue. More...
#include <rf_common_cmd.h>

Data Fields | |
| uint16_t | commandNo | 
| The command ID number 0x0007.  More... | |
| uint16_t | __dummy0 | 
| dataQueue_t * | pQueue | 
| Pointer to the queue structure to be flushed.  More... | |
| uint8_t * | pFirstEntry | 
| Pointer to the first entry that was removed.  More... | |
Flush Data Queue.
| uint16_t rfc_CMD_FLUSH_QUEUE_s::commandNo | 
The command ID number 0x0007.
| uint16_t rfc_CMD_FLUSH_QUEUE_s::__dummy0 | 
| dataQueue_t * rfc_CMD_FLUSH_QUEUE_s::pQueue | 
Pointer to the queue structure to be flushed.
| uint8_t * rfc_CMD_FLUSH_QUEUE_s::pFirstEntry | 
Pointer to the first entry that was removed.