![]()  | 
  ![]()  | 
| 
    rflib
    
   | 
 
#include <rf_prop_cmd.h>

Data Fields | |
| uint16_t | commandNo | 
| The command ID number.  More... | |
| uint16_t | status | 
| An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.  More... | |
| rfc_radioOp_t * | pNextOp | 
| Pointer to the next operation to run after this operation is done.  More... | |
| ratmr_t | startTime | 
Absolute or relative start time (depending on the value of startTrigger)  More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| struct { | |
| uint16_t modType:3 | |
| 0: FSK 1: GFSK 2: OOK Others: Reserved More...  | |
| uint16_t deviation:11 | |
Deviation (specified in number of steps, with step size given by deviationStepSz)  More... | |
| uint16_t deviationStepSz:2 | |
| Deviation step size 0: 250 Hz 1: 1000 Hz 2: 15.625 Hz 3: 62.5 Hz. More...  | |
| } | modulation | 
| struct { | |
| uint32_t preScale:8 | |
| Prescaler value.  More... | |
| uint32_t rateWord:21 | |
| Rate word.  More... | |
| uint32_t decimMode:3 | |
| 0: Use automatic PDIF decimation 1: Force PDIF decimation to 0 3: Force PDIF decimation to 1 5: Force PDIF decimation to 2 Others: Reserved More...  | |
| } | symbolRate | 
| Symbol rate setting.  More... | |
| uint8_t | rxBw | 
| Receiver bandwidth.  More... | |
| struct { | |
| uint8_t nPreamBytes:6 | |
| 0: 1 preamble bit 1–16: Number of preamble bytes 18, 20, ..., 30: Number of preamble bytes 31: 4 preamble bits 32: 32 preamble bytes Others: Reserved More...  | |
| uint8_t preamMode:2 | |
| 0: Send 0 as the first preamble bit 1: Send 1 as the first preamble bit 2: Send same first bit in preamble and sync word 3: Send different first bit in preamble and sync word More...  | |
| } | preamConf | 
| struct { | |
| uint16_t nSwBits:6 | |
| Number of sync word bits (8–32)  More... | |
| uint16_t bBitReversal:1 | |
| 0: Use positive deviation for 1 1: Use positive deviation for 0 More...  | |
| uint16_t bMsbFirst:1 | |
| 0: Least significant bit transmitted first 1: Most significant bit transmitted first More...  | |
| uint16_t fecMode:4 | |
| Select coding 0: Uncoded binary modulation 10: Manchester coded binary modulation Others: Reserved More...  | |
| uint16_t __pad0__:1 | |
| uint16_t whitenMode:3 | |
| 0: No whitening 1: CC1101/CC2500 compatible whitening 2: PN9 whitening without byte reversal 3: Reserved 4: No whitener, 32-bit IEEE 802.15.4g compatible CRC 5: IEEE 802.15.4g compatible whitener and 32-bit CRC 6: No whitener, dynamically IEEE 802.15.4g compatible 16-bit or 32-bit CRC 7: Dynamically IEEE 802.15.4g compatible whitener and 16-bit or 32-bit CRC More...  | |
| } | formatConf | 
| struct { | |
| uint16_t frontEndMode:3 | |
| 0x00: Differential mode 0x01: Single-ended mode RFP 0x02: Single-ended mode RFN 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX) 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX) Others: Reserved More...  | |
| uint16_t biasMode:1 | |
| 0: Internal bias 1: External bias More...  | |
| uint16_t analogCfgMode:6 | |
| 0x00: Write analog configuration. Required first time after boot and when changing frequency band or front-end configuration 0x2D: Keep analog configuration. May be used after standby or when changing mode with the same frequency band and front-end configuration Others: Reserved More...  | |
| uint16_t bNoFsPowerUp:1 | |
| 0: Power up frequency synth 1: Do not power up frequency synth More...  | |
| uint16_t __pad0__:1 | |
| uint16_t bSynthNarrowBand:1 | |
| 0: Normal synth mode 1: Narrow-band synth mode More...  | |
| } | config | 
| Configuration options.  More... | |
| uint16_t | txPower | 
| Transmit power.  More... | |
| uint32_t * | pRegOverride | 
| Pointer to a list of hardware and configuration registers to override. If NULL, no override is used.  More... | |
| uint16_t | centerFreq | 
| Center frequency of the frequency band used, in MHz; used for calculating some internal TX and RX parameters. For a single channel RF system, this should be set equal to the RF frequency used. For a multi channel RF system (e.g. frequency hopping spread spectrum), this should be set equal to the center frequency of the frequency band used.  More... | |
| int16_t | intFreq | 
| Intermediate frequency to use for RX, in MHz on 4.12 signed format. TX will use same intermediate frequency if supported, otherwise 0. 0x8000: Use default. More...  | |
| uint8_t | loDivider | 
| LO frequency divider setting to use. Supported values: 0, 2, 4, 5, 6, 10, 12, 15, and 30.  More... | |
| uint8_t | __dummy0 | 
| uint16_t | __dummy1 | 
| uint32_t * | pRegOverrideTxStd | 
| Pointer to a list of hardware and configuration registers to override when switching to standard PA. Used by RF driver only, not radio CPU.  More... | |
| uint32_t * | pRegOverrideTx20 | 
| Pointer to a list of hardware and configuration registers to override when switching to 20-dBm PA. Used by RF driver only, not radio CPU.  More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| struct { | |
| uint16_t modType:3 | |
| 0: FSK 1: GFSK 2: OOK Others: Reserved More...  | |
| uint16_t deviation:11 | |
Deviation (specified in number of steps, with step size given by deviationStepSz)  More... | |
| uint16_t deviationStepSz:2 | |
| Deviation step size 0: 250 Hz 1: 1000 Hz 2: 15.625 Hz 3: 62.5 Hz. More...  | |
| } | modulation | 
| struct { | |
| uint32_t preScale:8 | |
| Prescaler value.  More... | |
| uint32_t rateWord:21 | |
| Rate word.  More... | |
| uint32_t decimMode:3 | |
| 0: Use automatic PDIF decimation 1: Force PDIF decimation to 0 3: Force PDIF decimation to 1 5: Force PDIF decimation to 2 Others: Reserved More...  | |
| } | symbolRate | 
| Symbol rate setting.  More... | |
| struct { | |
| uint8_t nPreamBytes:6 | |
| 0: 1 preamble bit 1–16: Number of preamble bytes 18, 20, ..., 30: Number of preamble bytes 31: 4 preamble bits 32: 32 preamble bytes Others: Reserved More...  | |
| uint8_t preamMode:2 | |
| 0: Send 0 as the first preamble bit 1: Send 1 as the first preamble bit 2: Send same first bit in preamble and sync word 3: Send different first bit in preamble and sync word More...  | |
| } | preamConf | 
| struct { | |
| uint16_t nSwBits:6 | |
| Number of sync word bits (8–32)  More... | |
| uint16_t bBitReversal:1 | |
| 0: Use positive deviation for 1 1: Use positive deviation for 0 More...  | |
| uint16_t bMsbFirst:1 | |
| 0: Least significant bit transmitted first 1: Most significant bit transmitted first More...  | |
| uint16_t fecMode:4 | |
| Select coding 0: Uncoded binary modulation 10: Manchester coded binary modulation Others: Reserved More...  | |
| uint16_t __pad0__:1 | |
| uint16_t whitenMode:3 | |
| 0: No whitening 1: CC1101/CC2500 compatible whitening 2: PN9 whitening without byte reversal 3: Reserved 4: No whitener, 32-bit IEEE 802.15.4g compatible CRC 5: IEEE 802.15.4g compatible whitener and 32-bit CRC 6: No whitener, dynamically IEEE 802.15.4g compatible 16-bit or 32-bit CRC 7: Dynamically IEEE 802.15.4g compatible whitener and 16-bit or 32-bit CRC More...  | |
| } | formatConf | 
| struct { | |
| uint16_t frontEndMode:3 | |
| 0x00: Differential mode 0x01: Single-ended mode RFP 0x02: Single-ended mode RFN 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX) 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX) Others: Reserved More...  | |
| uint16_t biasMode:1 | |
| 0: Internal bias 1: External bias More...  | |
| uint16_t analogCfgMode:6 | |
| 0x00: Write analog configuration. Required first time after boot and when changing frequency band or front-end configuration 0x2D: Keep analog configuration. May be used after standby or when changing mode with the same frequency band and front-end configuration Others: Reserved More...  | |
| uint16_t bNoFsPowerUp:1 | |
| 0: Power up frequency synth 1: Do not power up frequency synth More...  | |
| uint16_t __pad0__:1 | |
| uint16_t bSynthNarrowBand:1 | |
| 0: Normal synth mode 1: Narrow-band synth mode More...  | |
| } | config | 
| Configuration options.  More... | |
| struct { | |
| uint8_t triggerType:4 | |
| The type of trigger.  More... | |
| uint8_t bEnaCmd:1 | |
| 0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More...  | |
| uint8_t triggerNo:2 | |
| The trigger number of the CMD_TRIGGER command that triggers this action.  More... | |
| uint8_t pastTrig:1 | |
| 0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More...  | |
| } | startTrigger | 
| Identification of the trigger that starts the operation.  More... | |
| struct { | |
| uint8_t rule:4 | |
| Condition for running next command: Rule for how to proceed.  More... | |
| uint8_t nSkip:4 | |
| Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...  More... | |
| } | condition | 
| struct { | |
| uint16_t modType:3 | |
| 0: FSK 1: GFSK 2: OOK Others: Reserved More...  | |
| uint16_t deviation:11 | |
Deviation (specified in number of steps, with step size given by deviationStepSz)  More... | |
| uint16_t deviationStepSz:2 | |
| Deviation step size 0: 250 Hz 1: 1000 Hz 2: 15.625 Hz 3: 62.5 Hz. More...  | |
| } | modulation | 
| struct { | |
| uint32_t preScale:8 | |
| Prescaler value.  More... | |
| uint32_t rateWord:21 | |
| Rate word.  More... | |
| uint32_t decimMode:3 | |
| 0: Use automatic PDIF decimation 1: Force PDIF decimation to 0 3: Force PDIF decimation to 1 5: Force PDIF decimation to 2 Others: Reserved More...  | |
| } | symbolRate | 
| Symbol rate setting.  More... | |
| struct { | |
| uint8_t nPreamBytes:6 | |
| 0: 1 preamble bit 1–16: Number of preamble bytes 18, 20, ..., 30: Number of preamble bytes 31: 4 preamble bits 32: 32 preamble bytes Others: Reserved More...  | |
| uint8_t preamMode:2 | |
| 0: Send 0 as the first preamble bit 1: Send 1 as the first preamble bit 2: Send same first bit in preamble and sync word 3: Send different first bit in preamble and sync word More...  | |
| } | preamConf | 
| struct { | |
| uint16_t nSwBits:6 | |
| Number of sync word bits (8–32)  More... | |
| uint16_t bBitReversal:1 | |
| 0: Use positive deviation for 1 1: Use positive deviation for 0 More...  | |
| uint16_t bMsbFirst:1 | |
| 0: Least significant bit transmitted first 1: Most significant bit transmitted first More...  | |
| uint16_t fecMode:4 | |
| Select coding 0: Uncoded binary modulation 10: Manchester coded binary modulation Others: Reserved More...  | |
| uint16_t __pad0__:1 | |
| uint16_t whitenMode:3 | |
| 0: No whitening 1: CC1101/CC2500 compatible whitening 2: PN9 whitening without byte reversal 3: Reserved 4: No whitener, 32-bit IEEE 802.15.4g compatible CRC 5: IEEE 802.15.4g compatible whitener and 32-bit CRC 6: No whitener, dynamically IEEE 802.15.4g compatible 16-bit or 32-bit CRC 7: Dynamically IEEE 802.15.4g compatible whitener and 16-bit or 32-bit CRC More...  | |
| } | formatConf | 
| struct { | |
| uint16_t frontEndMode:3 | |
| 0x00: Differential mode 0x01: Single-ended mode RFP 0x02: Single-ended mode RFN 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX) 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX) Others: Reserved More...  | |
| uint16_t biasMode:1 | |
| 0: Internal bias 1: External bias More...  | |
| uint16_t analogCfgMode:6 | |
| 0x00: Write analog configuration. Required first time after boot and when changing frequency band or front-end configuration 0x2D: Keep analog configuration. May be used after standby or when changing mode with the same frequency band and front-end configuration Others: Reserved More...  | |
| uint16_t bNoFsPowerUp:1 | |
| 0: Power up frequency synth 1: Do not power up frequency synth More...  | |
| uint16_t __pad0__:1 | |
| uint16_t bSynthNarrowBand:1 | |
| 0: Normal synth mode 1: Narrow-band synth mode More...  | |
| } | config | 
| Configuration options.  More... | |
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::commandNo | 
The command ID number.
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::status | 
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
| rfc_radioOp_t * rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::pNextOp | 
Pointer to the next operation to run after this operation is done.
| ratmr_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::startTime | 
Absolute or relative start time (depending on the value of startTrigger) 
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::triggerType | 
The type of trigger.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::bEnaCmd | 
0: No alternative trigger command
 1: CMD_TRIGGER can be used as an alternative trigger 
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::triggerNo | 
The trigger number of the CMD_TRIGGER command that triggers this action.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::pastTrig | 
0: A trigger in the past is never triggered, or for start of commands, give an error
 1: A trigger in the past is triggered as soon as possible 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::startTrigger | 
Identification of the trigger that starts the operation.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::rule | 
Condition for running next command: Rule for how to proceed.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::nSkip | 
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::condition | 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::modType | 
0: FSK
 1: GFSK
 2: OOK
 Others: Reserved 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::deviation | 
Deviation (specified in number of steps, with step size given by deviationStepSz) 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::deviationStepSz | 
Deviation step size
 0: 250 Hz
 1: 1000 Hz
 2: 15.625 Hz
 3: 62.5 Hz. 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::modulation | 
| uint32_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::preScale | 
Prescaler value.
| uint32_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::rateWord | 
Rate word.
| uint32_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::decimMode | 
0: Use automatic PDIF decimation
 1: Force PDIF decimation to 0
 3: Force PDIF decimation to 1
 5: Force PDIF decimation to 2
 Others: Reserved 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::symbolRate | 
Symbol rate setting.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::rxBw | 
Receiver bandwidth.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::nPreamBytes | 
0: 1 preamble bit
 1–16: Number of preamble bytes
 18, 20, ..., 30: Number of preamble bytes
 31: 4 preamble bits
 32: 32 preamble bytes
 Others: Reserved 
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::preamMode | 
0: Send 0 as the first preamble bit
 1: Send 1 as the first preamble bit
 2: Send same first bit in preamble and sync word
 3: Send different first bit in preamble and sync word 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::preamConf | 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::nSwBits | 
Number of sync word bits (8–32)
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::bBitReversal | 
0: Use positive deviation for 1
 1: Use positive deviation for 0 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::bMsbFirst | 
0: Least significant bit transmitted first
 1: Most significant bit transmitted first 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::fecMode | 
Select coding
 0: Uncoded binary modulation
 10: Manchester coded binary modulation
 Others: Reserved 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::__pad0__ | 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::whitenMode | 
0: No whitening
 1: CC1101/CC2500 compatible whitening
 2: PN9 whitening without byte reversal
 3: Reserved
 4: No whitener, 32-bit IEEE 802.15.4g compatible CRC
 5: IEEE 802.15.4g compatible whitener and 32-bit CRC
 6: No whitener, dynamically IEEE 802.15.4g compatible 16-bit or 32-bit CRC
 7: Dynamically IEEE 802.15.4g compatible whitener and 16-bit or 32-bit CRC 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::formatConf | 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::frontEndMode | 
0x00: Differential mode
 0x01: Single-ended mode RFP
 0x02: Single-ended mode RFN
 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX)
 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX)
 Others: Reserved 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::biasMode | 
0: Internal bias
 1: External bias 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::analogCfgMode | 
0x00: Write analog configuration.
 Required first time after boot and when changing frequency band or front-end configuration
 0x2D: Keep analog configuration.
 May be used after standby or when changing mode with the same frequency band and front-end configuration
 Others: Reserved 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::bNoFsPowerUp | 
0: Power up frequency synth
 1: Do not power up frequency synth 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::bSynthNarrowBand | 
0: Normal synth mode
 1: Narrow-band synth mode 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::config | 
Configuration options.
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::txPower | 
Transmit power.
| uint32_t * rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::pRegOverride | 
Pointer to a list of hardware and configuration registers to override. If NULL, no override is used.
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::centerFreq | 
Center frequency of the frequency band used, in MHz; used for calculating some internal TX and RX parameters. For a single channel RF system, this should be set equal to the RF frequency used. For a multi channel RF system (e.g. frequency hopping spread spectrum), this should be set equal to the center frequency of the frequency band used.
| int16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::intFreq | 
Intermediate frequency to use for RX, in MHz on 4.12 signed format. TX will use same intermediate frequency if supported, otherwise 0.
 0x8000: Use default. 
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::loDivider | 
LO frequency divider setting to use. Supported values: 0, 2, 4, 5, 6, 10, 12, 15, and 30.
| uint8_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::__dummy0 | 
| uint16_t rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::__dummy1 | 
| uint32_t * rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::pRegOverrideTxStd | 
Pointer to a list of hardware and configuration registers to override when switching to standard PA. Used by RF driver only, not radio CPU.
| uint32_t * rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::pRegOverrideTx20 | 
Pointer to a list of hardware and configuration registers to override when switching to 20-dBm PA. Used by RF driver only, not radio CPU.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::startTrigger | 
Identification of the trigger that starts the operation.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::condition | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::modulation | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::symbolRate | 
Symbol rate setting.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::preamConf | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::formatConf | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::config | 
Configuration options.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::startTrigger | 
Identification of the trigger that starts the operation.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::condition | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::modulation | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::symbolRate | 
Symbol rate setting.
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::preamConf | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::formatConf | 
| struct { ... } rfc_CMD_PROP_RADIO_DIV_SETUP_PA_s::config | 
Configuration options.