FCC Certification Considerations

This section will cover important TI 15.4-Stack application changes which may be required to achieve FCC certification given a specific hardware design.

Power Limiting Table Adjustment

Some LaunchPad designs are known to fail FCC certifications at higher 2.4 GHz channels due to increased second harmonic transmissions. In order to work around this issue, a power limiting table PowerLimitTableIeee has been initialized inside mac_user_config.c to help limit the maximum transmission level for channels which are known to be affected.

/*
* For CC1352P_2_LAUNCHXL, set ch25 to 19dBm and ch26 to 15dBm
*
* For LP_CC2652RSIP, set all ch to 5dBm except for 26, set ch26 to 2dBm
*
* For LP_CC2652PSIP, set ch26 to 2dBm and set other ch to 10dBm
*/
int8_t PowerLimitTableIeee[RF_CONFIG_IEEE_PL_NO_CHANNELS] =
{
    20,    //20dBm max for Channel = 11
    20,    //20dBm max for Channel = 12
    20,    //20dBm max for Channel = 13
    20,    //20dBm max for Channel = 14
    20,    //20dBm max for Channel = 15
    20,    //20dBm max for Channel = 16
    20,    //20dBm max for Channel = 17
    20,    //20dBm max for Channel = 18
    20,    //20dBm max for Channel = 19
    20,    //20dBm max for Channel = 20
    20,    //20dBm max for Channel = 21
    20,    //20dBm max for Channel = 22
    20,    //20dBm max for Channel = 23
    20,    //20dBm max for Channel = 24
    19,    //19dBm max for Channel = 25
    15,    //15dBm max for Channel = 26
};

The example above provides the correct power limit table changes necessary based on existing FCC certification of the LAUNCHXL-CC1352P-2, and a comprehensive list of other affected LaunchPads is provided in the table below. If FCC certification is desired for any of these LaunchPads, their respective mac_user_config.c files’s PowerLimitTableIeee must be modified to compensate.

Table 24. Power Limit Table Entries for affected Launchpads

LaunchPad

Channel

Entry

CC1352P_2_LAUNCHXL

25, 26

19, 15

LP_CC2652RSIP

26

2

LP_CC2652PSIP

11-25, 26

10, 2

LP_CC2651R3SIPA

26

1

Note

Power limitation values will vary slightly for each custom hardware design, thus caution should be taken to identify the optimal values during FCC certification and modify the table accordingly

CC1312PSIP FCC Module Certification

In order to re-use the FCC RF Module certification of CC1312PSIP on Sub 1GHz channels, an application using TI 15.4 stack (in Frequency Hopping mode) or TI Wi-SUN FAN stack needs to limit the transmit power to the following values. If you set the transmit power to more than the values stated in the following tables, you need to re-certify the product and will likely pass only with duty cycling.

Table 25. Power Limits for TI 15.4 stack on 20 dBm PA

Stack

Tx Power

Additional Condition

TI 15.4 Stack

19 dBm

If you only use channels between 908.2-927MHz

TI 15.4 Stack

16 dBm

If you include any channel between 902.2-908MHz

Table 26. Power Limits for TI Wi-SUN FAN Stack on 20 dBm PA

Stack

Tx Power

Additional Condition

TI Wi-SUN FAN Stack

19 dBm

If you duty cycle with 60ms out of 100ms in TX

TI Wi-SUN FAN Stack

17 dBm

Without duty cycling

If you are using other certified PHYs, you will find the limits in the following tables.

Table 27. Power limits for WB-DSSS PHYs on 20 dBm PA

Phy

Tx Power

Additional Condition

WB-DSSS All Phys

15 dBm

Under all conditions

Table 28. Power limits for MIOTY PHYs on 20 dBm PA

Phy

Tx Power

Additional Condition

MIOTY

20 dBm

If you duty cycle with 60ms out of 100ms in TX

MIOTY

19 dBm

Without duty cycling

If you are using the 14 dBm port, the following table provides the maximum TX power that you can set during transmission in order to re-use the FCC RF Module certification of CC1312PSIP on Sub 1GHz channels. It is not necessary to use duty cycling or modify channel plans in this case.

Table 29. Power limits for all certified PHYs on 14 dBm PA

Phy/Stack

Tx Power

TI 15.4 Stack

12.5 dBm

TI Wi-SUN FAN Stack

12.5 dBm

WB-DSSS PHYs

12.5 dBm

MIOTY PHYs

12.5 dBm