![]() |
![]() |
|
TI-15.4 Stack API
|
#include <api_mac.h>

Data Fields | |
| ApiMac_sec_t | sec |
| ApiMac_sAddr_t | deviceAddress |
| uint16_t | devicePanId |
| ApiMac_disassocateReason_t | disassociateReason |
| bool | txIndirect |
MLME disassociate request type
| ApiMac_sec_t _apimac_mlmedisassociatereq::sec |
The security parameters for this message
| ApiMac_sAddr_t _apimac_mlmedisassociatereq::deviceAddress |
The address of the device with which to disassociate
| uint16_t _apimac_mlmedisassociatereq::devicePanId |
The PAN ID of the device
| ApiMac_disassocateReason_t _apimac_mlmedisassociatereq::disassociateReason |
The disassociate reason
| bool _apimac_mlmedisassociatereq::txIndirect |
Transmit Indirect