TI-15.4 Stack API
Data Fields
_apimac_mlmeorphanrsp Struct Reference

#include <api_mac.h>

Collaboration diagram for _apimac_mlmeorphanrsp:
Collaboration graph
[legend]

Data Fields

ApiMac_sec_t sec
 
ApiMac_sAddrExt_t orphanAddress
 
uint16_t shortAddress
 
bool associatedMember
 

Detailed Description

MLME orphan response type

Field Documentation

§ sec

ApiMac_sec_t _apimac_mlmeorphanrsp::sec

The security parameters for this message

§ orphanAddress

ApiMac_sAddrExt_t _apimac_mlmeorphanrsp::orphanAddress

The extended address of the device sending the orphan notification

§ shortAddress

uint16_t _apimac_mlmeorphanrsp::shortAddress

The short address of the orphaned device

§ associatedMember

bool _apimac_mlmeorphanrsp::associatedMember

TRUE if the orphaned device is associated with this coordinator


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale