SYS/BIOS  7.00
Data Structures | Macros | Typedefs | Functions
HeapTrack.h File Reference

Detailed Description

Heap manager that enables tracking of all allocated blocks.

HeapTrack manager provides functions to allocate and free storage from a configured heap which inherits from IHeap. The calling context is going to match the heap being used.

HeapTrack is useful for detecting memory leaks, double frees and buffer overflows. There is a performance overhead cost when using heap track as well as a size impact. Every alloc will include a HeapTrack_Tracker structure (plus memory to get proper alignment of the stucture) at the end of the buffer that should not be modified by the user. It is important to remember this when deciding on heap sizes and you may have to adjust the total size or buffer sizes (for HeapBuf/HeapMultiBuf).

ROV displays peaks and current in-use for both allocated memory (requested size + Tracker structure) and requested memory (without Tracker).

The information stored in the tracker packet is used to display information in RTOS Object Viewer (ROV) as well as with the printTask and printHeap functions.

The asserts used in this module are listed below and include error checking for double frees, calling printHeap with a null handle, buffer overflows and deleting a non empty heap.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/knl/Queue.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/runtime/Error.h>
#include <ti/sysbios/runtime/IHeap.h>
#include <ti/sysbios/runtime/Memory.h>
Include dependency graph for HeapTrack.h:

Go to the source code of this file.

Data Structures

struct  HeapTrack_Tracker
 Structure added to the end of each allocated block. More...
 
struct  HeapTrack_Params
 
struct  HeapTrack_Struct
 
struct  HeapTrack_Module_State
 

Macros

#define HeapTrack_A_doubleFree   "Buffer already free"
 Assert raised when freeing a buffer that was already freed. More...
 
#define HeapTrack_A_bufOverflow   "Buffer overflow"
 Assert raised when freeing memory with corrupted data or using the wrong size. More...
 
#define HeapTrack_A_notEmpty   "Heap not empty"
 Assert raised when deleting a non-empty heap. More...
 
#define HeapTrack_A_nullObject   "HeapTrack_printHeap called with null obj"
 Assert raised when calling printTask with a null HeapTrack object. More...
 
#define ti_sysbios_heaps_HeapTrack_Handle_upCast(handle)   ((IHeap_Handle)(handle))
 cast handle to an IHeap_Handle for use by Memory_alloc, etc. More...
 

Typedefs

typedef struct HeapTrack_StructHeapTrack_Handle
 
typedef HeapTrack_Struct HeapTrack_Object
 

Functions

void * HeapTrack_alloc (HeapTrack_Handle heap, size_t size, size_t align, Error_Block *eb)
 Allocate a block of memory from the heap. More...
 
void HeapTrack_free (HeapTrack_Handle heap, void *buf, size_t size)
 Free a block of memory back to the heap. More...
 
bool HeapTrack_isBlocking (HeapTrack_Handle heap)
 Can this heap block the caller. More...
 
void HeapTrack_getStats (HeapTrack_Handle heap, Memory_Stats *stats)
 get memory stats for a HeapTrack object More...
 
void HeapTrack_printTask (Task_Handle task)
 Print out the blocks that are currently allocated by a task. More...
 
void HeapTrack_printHeap (HeapTrack_Handle heap)
 Print details for a HeapTrack instance. More...
 
HeapTrack_Handle HeapTrack_Object_first (void)
 return handle of the first HeapTrack on HeapTrack list More...
 
HeapTrack_Handle HeapTrack_Object_next (HeapTrack_Handle heap)
 return handle of the next HeapTrack on HeapTrack list More...
 
HeapTrack_Handle HeapTrack_create (const HeapTrack_Params *params, Error_Block *eb)
 Create a HeapTrack heap. More...
 
HeapTrack_Handle HeapTrack_construct (HeapTrack_Struct *obj, const HeapTrack_Params *params)
 Construct a HeapTrack heap. More...
 
void HeapTrack_delete (HeapTrack_Handle *heap)
 Delete a HeapTrack heap. More...
 
void HeapTrack_destruct (HeapTrack_Struct *obj)
 Destruct a HeapTrack heap. More...
 
void HeapTrack_Params_init (HeapTrack_Params *prms)
 Initialize the HeapTrack_Params structure with default values. More...
 
static HeapTrack_Handle HeapTrack_handle (HeapTrack_Struct *str)
 
static HeapTrack_StructHeapTrack_struct (HeapTrack_Handle h)
 

Macro Definition Documentation

§ HeapTrack_A_doubleFree

#define HeapTrack_A_doubleFree   "Buffer already free"

Assert raised when freeing a buffer that was already freed.

§ HeapTrack_A_bufOverflow

#define HeapTrack_A_bufOverflow   "Buffer overflow"

Assert raised when freeing memory with corrupted data or using the wrong size.

§ HeapTrack_A_notEmpty

#define HeapTrack_A_notEmpty   "Heap not empty"

Assert raised when deleting a non-empty heap.

§ HeapTrack_A_nullObject

#define HeapTrack_A_nullObject   "HeapTrack_printHeap called with null obj"

Assert raised when calling printTask with a null HeapTrack object.

§ ti_sysbios_heaps_HeapTrack_Handle_upCast

#define ti_sysbios_heaps_HeapTrack_Handle_upCast (   handle)    ((IHeap_Handle)(handle))

cast handle to an IHeap_Handle for use by Memory_alloc, etc.

Parameters
handleheap handle
Return values
IHeap_Handle

Typedef Documentation

§ HeapTrack_Handle

§ HeapTrack_Object

Function Documentation

§ HeapTrack_alloc()

void* HeapTrack_alloc ( HeapTrack_Handle  heap,
size_t  size,
size_t  align,
Error_Block eb 
)

Allocate a block of memory from the heap.

Precondition
The alignment must be a power of 2.

§ HeapTrack_free()

void HeapTrack_free ( HeapTrack_Handle  heap,
void *  buf,
size_t  size 
)

Free a block of memory back to the heap.

§ HeapTrack_isBlocking()

bool HeapTrack_isBlocking ( HeapTrack_Handle  heap)

Can this heap block the caller.

HeapTrack returns true if the underlying heap is blocking. HeapTrack returns false if the underlying heap not blocking.

Parameters
heapheap handle
Return values
<tt>true</tt>if the underlying heap if blocking, false otherwise

§ HeapTrack_getStats()

void HeapTrack_getStats ( HeapTrack_Handle  heap,
Memory_Stats stats 
)

get memory stats for a HeapTrack object

Parameters
heapheap handle
statspointer to a Memory_Stats object

§ HeapTrack_printTask()

void HeapTrack_printTask ( Task_Handle  task)

Print out the blocks that are currently allocated by a task.

Iterates through all instances of HeapTrack and prints out information about all allocated blocks of memory for a given task handle. This function is not thread safe.

§ HeapTrack_printHeap()

void HeapTrack_printHeap ( HeapTrack_Handle  heap)

Print details for a HeapTrack instance.

Print the details of all allocated blocks of memory for a HeapTrack instance. This function is not thread safe.

§ HeapTrack_Object_first()

HeapTrack_Handle HeapTrack_Object_first ( void  )

return handle of the first HeapTrack on HeapTrack list

Return the handle of the first HeapTrack on the create/construct list. NULL if no HeapTracks have been created or constructed.

Return values
HeapTrackhandle

§ HeapTrack_Object_next()

HeapTrack_Handle HeapTrack_Object_next ( HeapTrack_Handle  heap)

return handle of the next HeapTrack on HeapTrack list

Return the handle of the next HeapTrack on the create/construct list. NULL if no more HeapTracks are on the list.

Parameters
heapHeapTrack handle
Return values
HeapTrackhandle

§ HeapTrack_create()

HeapTrack_Handle HeapTrack_create ( const HeapTrack_Params params,
Error_Block eb 
)

Create a HeapTrack heap.

Parameters
paramsoptional parameters
eberror block
Return values
HeapTrackhandle (NULL on failure)

§ HeapTrack_construct()

HeapTrack_Handle HeapTrack_construct ( HeapTrack_Struct obj,
const HeapTrack_Params params 
)

Construct a HeapTrack heap.

HeapTrack_construct is equivalent to HeapTrack_create except that the HeapTrack_Struct is pre-allocated.

Parameters
objpointer to a HeapTrack object
paramsoptional parameters
Return values
HeapTrackhandle (NULL on failure)

§ HeapTrack_delete()

void HeapTrack_delete ( HeapTrack_Handle heap)

Delete a HeapTrack heap.

Note that HeapTrack_delete takes a pointer to a HeapTrack_Handle which enables HeapTrack_delete to set the HeapTrack handle to NULL.

Parameters
heappointer to a HeapTrack handle

§ HeapTrack_destruct()

void HeapTrack_destruct ( HeapTrack_Struct obj)

Destruct a HeapTrack heap.

Parameters
objpointer to a HeapTrack objects

§ HeapTrack_Params_init()

void HeapTrack_Params_init ( HeapTrack_Params prms)

Initialize the HeapTrack_Params structure with default values.

HeapTrack_Params_init initializes the HeapTrack_Params structure with default values. HeapTrack_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

Parameters
prmspointer to uninitialized params structure

§ HeapTrack_handle()

static HeapTrack_Handle HeapTrack_handle ( HeapTrack_Struct str)
inlinestatic

§ HeapTrack_struct()

static HeapTrack_Struct* HeapTrack_struct ( HeapTrack_Handle  h)
inlinestatic
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale