SYS/BIOS  7.00
Data Structures | Typedefs | Functions
Queue.h File Reference

Detailed Description

Queue Manager.

The Queue module makes available a set of functions that manipulate queue objects accessed through handles of type Queue_Handle. Each queue contains a linked sequence of zero or more elements referenced through variables of type Queue_Elem, which are embedded as the first field within a structure.

In the Queue API descriptions, the APIs which disable interrupts before modifying the Queue are noted as "atomic", while APIs that do not disable interrupts are "non-atomic".

Queues are represented as doubly-linked lists, so calls to Queue_next or Queue_prev can loop continuously over the Queue. The following code demonstrates one way to iterate over a Queue once from beginning to end. In this example, 'myQ' is a Queue_Handle.

Queue_Elem *elem;
for (elem = Queue_head(myQ);
elem != (Queue_Elem *)myQ;
elem = Queue_next(elem)) {
...
}

Below is a simple example of how to create a Queue, enqueue two elements, and dequeue the elements until the queue is empty:

#include <xdc/std.h>
#include <xdc/runtime/System.h>
typedef struct Rec {
Queue_Elem _elem;
int data;
} Rec;
int main(int argc, char *argv[])
{
Rec r1, r2;
Rec* rp;
r1.data = 100;
r2.data = 200;
// create a Queue instance 'q'
q = Queue_create(NULL, NULL);
// enQ a couple of records
Queue_enqueue(q, &r1._elem);
Queue_enqueue(q, &r2._elem);
// deQ the records and print their data values until Q is empty
while (!Queue_empty(q)) {
rp = Queue_dequeue(q);
System_printf("rec: %d\n", rp->data);
}
return (0);
}

Unconstrained Functions All functions are unconstrained

Calling Context

Function Hwi Swi Task Main Startup
Queue_create N N Y Y N
Queue_insert Y Y Y Y N
Queue_next Y Y Y Y N
Queue_Params_init Y Y Y Y N
Queue_prev Y Y Y Y N
Queue_remove Y Y Y Y N
Queue_construct Y Y Y Y N
Queue_delete N N Y Y N
Queue_dequeue Y Y Y Y N
Queue_destruct Y Y Y Y N
Queue_empty Y Y Y Y N
Queue_enqueue Y Y Y Y N
Queue_get Y Y Y Y N
Queue_head Y Y Y Y N
Queue_put Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Queue_Module_startupDone() returns true).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Queue_Module_startupDone() returns false).

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Error.h>
Include dependency graph for Queue.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Queue_Elem
 Opaque queue element. More...
 
struct  Queue_Params
 

Typedefs

typedef struct Queue_Elem Queue_Elem
 Opaque queue element. More...
 
typedef Queue_Elem Queue_Struct
 
typedef Queue_Struct Queue_Object
 
typedef Queue_StructQueue_Handle
 

Functions

Queue_Handle Queue_create (const Queue_Params *prms, Error_Block *eb)
 Create a Queue object. More...
 
Queue_Handle Queue_construct (Queue_Struct *obj, const Queue_Params *prms)
 Construct a queue. More...
 
void Queue_delete (Queue_Handle *queue)
 Delete a queue. More...
 
void Queue_destruct (Queue_Struct *obj)
 Destruct a queue. More...
 
void Queue_Params_init (Queue_Params *prms)
 Initialize the Queue_Params structure with default values. More...
 
void Queue_insert (Queue_Elem *qelem, Queue_Elem *elem)
 Insert elem in the queue in front of qelem. More...
 
void * Queue_next (Queue_Elem *qelem)
 Return next element in queue (non-atomically). More...
 
void * Queue_prev (Queue_Elem *qelem)
 Return previous element in queue (non-atomically). More...
 
void Queue_remove (Queue_Elem *qelem)
 Remove qelem from middle of queue (non-atomically). More...
 
void * Queue_dequeue (Queue_Handle queue)
 Remove the element from the front of queue and return elem (non- atomically). More...
 
bool Queue_empty (Queue_Handle queue)
 Test for an empty queue. More...
 
void Queue_enqueue (Queue_Handle queue, Queue_Elem *elem)
 Insert at end of queue (non-atomically). More...
 
void * Queue_get (Queue_Handle queue)
 Get element from front of queue (atomically). More...
 
void * Queue_getTail (Queue_Handle queue)
 Get the element at the end of the queue (atomically). More...
 
void * Queue_head (Queue_Handle queue)
 Return element at front of queue. (atomically) More...
 
void Queue_put (Queue_Handle queue, Queue_Elem *elem)
 Put element at end of queue (atomically). More...
 
void Queue_putHead (Queue_Handle queue, Queue_Elem *elem)
 Put element at the front of the queue (atomically). More...
 

Typedef Documentation

§ Queue_Elem

typedef struct Queue_Elem Queue_Elem

Opaque queue element.

A field of this type is placed at the head of client structs.

§ Queue_Struct

§ Queue_Object

§ Queue_Handle

Function Documentation

§ Queue_create()

Queue_Handle Queue_create ( const Queue_Params prms,
Error_Block eb 
)

Create a Queue object.

This function creates a new Queue object.

Parameters
prmsqueue parameters
eberror block
Return values
Queuehandle (NULL on failure)

§ Queue_construct()

Queue_Handle Queue_construct ( Queue_Struct obj,
const Queue_Params prms 
)

Construct a queue.

Queue_construct is equivalent to Queue_create except that the Queue_Struct is pre-allocated. See Queue_create() for a description of this API.

Parameters
objpointer to a Queue object
prmsqueue parameters
Return values
Queuehandle (NULL on failure)

§ Queue_delete()

void Queue_delete ( Queue_Handle queue)

Delete a queue.

Queue_delete deletes a Queue object. Note that Queue_delete takes a pointer to a Queue_Handle which enables Queue_delete to set the Queue_handle to NULL.

Parameters
queuepointer to Task handle

§ Queue_destruct()

void Queue_destruct ( Queue_Struct obj)

Destruct a queue.

Queue_destruct destructs a Queue object.

Parameters
objpointer to Queue object

§ Queue_Params_init()

void Queue_Params_init ( Queue_Params prms)

Initialize the Queue_Params structure with default values.

Queue_Params_init initializes the Queue_Params structure with default values. Queue_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

Parameters
prmspointer to uninitialized params structure

§ Queue_insert()

void Queue_insert ( Queue_Elem qelem,
Queue_Elem elem 
)

Insert elem in the queue in front of qelem.

Parameters
qelemelement already in queue
elemelement to be inserted in queue

§ Queue_next()

void* Queue_next ( Queue_Elem qelem)

Return next element in queue (non-atomically).

This function returns a pointer to an Elem object in the queue after qelem. A Queue is represented internally as a doubly-linked list, so 'next' can be called in a continuous loop over the queue. See the module description for an example of iterating once over a Queue.

Parameters
qelemelement in queue
Return values
nextelement in queue

§ Queue_prev()

void* Queue_prev ( Queue_Elem qelem)

Return previous element in queue (non-atomically).

This function returns a pointer to an Elem object in the queue before qelem. A Queue is represented internally as a doubly-linked list, so 'prev' can be called in a continuous loop over the queue. See the module description for an example of iterating once over a Queue.

Parameters
qelemelement in queue
Return values
previouselement in queue

§ Queue_remove()

void Queue_remove ( Queue_Elem qelem)

Remove qelem from middle of queue (non-atomically).

The qelem parameter is a pointer to an existing element to be removed from the Queue.

Parameters
qelemelement in queue

§ Queue_dequeue()

void* Queue_dequeue ( Queue_Handle  queue)

Remove the element from the front of queue and return elem (non- atomically).

This function removes an element from the front of a queue and returns it.

If called with an empty queue, this function will return a pointer to the queue itself.

Note
empty Queue as shown in Queue_get() isn't reliable in a multi-threaded system. Thread safety can be achieved as shown below:
key = Hwi_disable();
if ((Queue_Handle)(elem = Queue_dequeue(q)) != q) {
` process elem `
}
Parameters
queueQueue handle
Return values
pointerto former first element

§ Queue_empty()

bool Queue_empty ( Queue_Handle  queue)

Test for an empty queue.

Parameters
queueQueue handle
Return values
trueif this queue is empty

§ Queue_enqueue()

void Queue_enqueue ( Queue_Handle  queue,
Queue_Elem elem 
)

Insert at end of queue (non-atomically).

Parameters
queueQueue handle
elempointer to an element

§ Queue_get()

void* Queue_get ( Queue_Handle  queue)

Get element from front of queue (atomically).

This function removes an element from the front of a queue and returns it.

If called with an empty queue, this function will return a pointer to the queue itself. This provides a means for using a single atomic action to check if a queue is empty, and to remove and return the first element if it is not empty:

if ((Queue_Handle)(elem = Queue_get(q)) != q) {
` process elem `
}
Parameters
queueQueue handle
Return values
pointerto former first element

§ Queue_getTail()

void* Queue_getTail ( Queue_Handle  queue)

Get the element at the end of the queue (atomically).

This function removes the element at the end of a queue and returns a pointer to it. If called with an empty queue, this function will return a pointer to the queue itself. This provides a means for using a single atomic action to check if a queue is empty, and to remove and return the last element if it is not empty:

if ((Queue_Handle)(elem = Queue_getTail(q)) != q) {
`process elem`
}
Parameters
queueQueue handle
Return values
pointerto former end element

§ Queue_head()

void* Queue_head ( Queue_Handle  queue)

Return element at front of queue. (atomically)

This function returns a pointer to the element at the front of a queue. The element is not removed from the queue. If called with an empty queue, this function will return a pointer to the queue itself. This provides a means for using a single atomic action to check if a queue is empty, and to return a pointer to the first element if it is not empty:

if ((Queue_Handle)(elem = Queue_head(q)) != q) {
`process elem`
Parameters
queueQueue handle
Return values
pointerto first element

§ Queue_put()

void Queue_put ( Queue_Handle  queue,
Queue_Elem elem 
)

Put element at end of queue (atomically).

Parameters
queueQueue handle
elempointer to new queue element

§ Queue_putHead()

void Queue_putHead ( Queue_Handle  queue,
Queue_Elem elem 
)

Put element at the front of the queue (atomically).

Parameters
queueQueue handle
elempointer to new queue element
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale