SYS/BIOS  7.00
Functions | Variables
Hwi.h File Reference

Detailed Description

Hwi header file for the HAL.

This module contains definitions for the static inline Hwi functions.

#include <xdc/std.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Types.h>
Include dependency graph for Hwi.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

void Hwi_switchAndRunFunc (void(*func)(void))
 
static unsigned int Hwi_disable ()
 
static unsigned int Hwi_enable ()
 
static void Hwi_restore (unsigned int key)
 

Variables

const unsigned int Hwi_disablePriority
 

Function Documentation

§ Hwi_switchAndRunFunc()

void Hwi_switchAndRunFunc ( void(*)(void)  func)

§ Hwi_disable()

static unsigned int Hwi_disable ( )
inlinestatic

§ Hwi_enable()

static unsigned int Hwi_enable ( )
inlinestatic

§ Hwi_restore()

static void Hwi_restore ( unsigned int  key)
inlinestatic

Variable Documentation

§ Hwi_disablePriority

const unsigned int Hwi_disablePriority
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale