Z-Stack API Reference  8.31.00.00
_zstack_afconfigsetreq_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t endpoint
 Endpoint.
 
uint8_t frameDelay
 Fragmentation frame delay.
 
uint8_t windowSize
 Fragmentation window size.
 

Detailed Description

Send this message to the ZStack Server to set the AF/APS Fragmentation parameters. The command ID for this message is AF_CONFIG_SET_REQ. The synchronous response to this message is zstack_DefaultRsp_t(cmdID:AF_CONFIG_SET_REQ).


The documentation for this struct was generated from the following file: