Z-Stack API Reference  8.31.00.00
_zstack_devforcemacparamsreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t nwkAddr
 Network address.
 
uint16_t panID
 device's PAN ID
 
uint8_t logicalChannel
 Logical Channel.
 

Detailed Description

Structure to send a Device Force MAC parameters Request.


The documentation for this struct was generated from the following file: