Z-Stack API Reference  8.31.00.00
_zstack_gpCommissioningMode_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t isEntering
 
uint8_t hasTime
 
uint16_t time
 

Detailed Description

Structure of Green Power Commissioning Mode.

Field Documentation

§ hasTime

uint8_t hasTime

The flag for commissioning time

§ isEntering

uint8_t isEntering

The flag to enter in commissioning mode

§ time

uint16_t time

The commissioning timeout


The documentation for this struct was generated from the following file: