![]()  | 
  ![]()  | 
| 
    Z-Stack API Reference
    8.31.00.00
    
   | 
 
#include <zstack.h>
Data Fields | |
| gpdID_t | gpdID | 
| uint8_t | EndPoint | 
| gp_SecData_t | gp_SecData | 
| uint8_t | dGPStubHandle | 
Structure to send a GP Security Request.
| uint8_t EndPoint | 
The identifier of the GPD endpoint used in combination with the GPD IEEE address if ApplicationID = 0b010. If ApplicationID = 0b000 this parameter is ignored
| gp_SecData_t gp_SecData | 
Security parameters
| gpdID_t gpdID | 
Green power device ID parameters