Z-Stack API Reference  8.31.00.00
ProxyTableEntryFormat_t Struct Reference

Data Fields

uint16_t options
 options. More...
 
uint32_t gpdId
 ID of the GPD.
 
uint8_t endPoint
 GPD endpoint.
 
uint16_t gpdAssignedAlias
 be used as alias for this GPD. More...
 
uint8_t securityOptions
 The security options.
 
uint32_t gpdSecurityFramecounter
 counter for the GPD. More...
 
uint8_t gpdKey [SEC_KEY_LEN]
 The security key for the GPD.
 
uint8_t * pLightweightSinkAddressList
 IEEE and short address of the sink.
 
uint8_t * pSinkGroupList
 
uint8_t groupcastRadius
 To limit the range of the group-cast.
 
uint8_t SearchCounter
 
uint16_t ExtendedOptions
 exten-sions to the tunneling options. More...
 
uint8_t * pFullUnicastSinkAddressList
 IEEE and short address of the sink.
 

Field Documentation

§ ExtendedOptions

uint16_t ExtendedOptions

exten-sions to the tunneling options.

This parameter specifies

§ gpdAssignedAlias

uint16_t gpdAssignedAlias

be used as alias for this GPD.

The commissioned 16-bit ID to

§ gpdSecurityFramecounter

uint32_t gpdSecurityFramecounter

counter for the GPD.

The incoming security frame

§ options

uint16_t options

options.

This parameter specifies the tunneling

§ pSinkGroupList

uint8_t* pSinkGroupList

GroupIDs and Aliases for the sinks that require the tunneling in groupcast communication mode.

§ SearchCounter

uint8_t SearchCounter

For inactive/invalid entries, allows for Sink re-discovery when Search Counter equals 0.


The documentation for this struct was generated from the following file: