Z-Stack API Reference  8.31.00.00
zclCommandRec_t Struct Reference

Command record. More...

#include <zcl.h>

Data Fields

uint16_t clusterID
 Cluster ID.
 
uint8_t cmdID
 Command ID.
 
uint8_t flag
 one of CMD_DIR_CLIENT_GENERATED, CMD_DIR_CLIENT_RECEIVED, CMD_DIR_SERVER_GENERATED, CMD_DIR_SERVER_RECEIVED
 

Detailed Description

Command record.


The documentation for this struct was generated from the following file: