Z-Stack API Reference  8.31.00.00
zclDoorLockSchedule_t Struct Reference

Server Commands Received: Get Week Day Schedule, Clear Week Day Schedule, Get Year Day Schedule, Clear Year Day Schedule. More...

#include <zcl_closures.h>

Data Fields

uint8_t scheduleID
 number is between 0 - [# of Week Day Schedules Per User attribute].
 
uint16_t userID
 is between 0 - [# of Total Users Supported attribute].
 

Detailed Description

Server Commands Received: Get Week Day Schedule, Clear Week Day Schedule, Get Year Day Schedule, Clear Year Day Schedule.


The documentation for this struct was generated from the following file: