Z-Stack API Reference  8.31.00.00
zclDoorLockSetUserType_t Struct Reference

Server Commands Received: Set User Type. More...

#include <zcl_closures.h>

Data Fields

uint16_t userID
 User ID is between 0 - [# of PIN Users Supported attribute].
 
uint8_t userType
 e.g. USER_TYPE_UNRESTRICTED_USER
 

Detailed Description

Server Commands Received: Set User Type.


The documentation for this struct was generated from the following file: