Z-Stack API Reference  8.31.00.00
zclGpCommissioningNotification_t Struct Reference

Data Fields

gpCommissioningNotificationOptions_t options
 Commissioning notification options bitfield.
 
gpdID_t gpdId
 Address identifier structure for Green Power Device.
 
uint8_t GPDEndpoint
 Endpoint of the GP if application ID is 0b010.
 
uint32_t securityFrameCounter
 Security frame counter from Green Power Device frame.
 
uint8_t gpCmdId
 GreenPower Command Id.
 
uint8_t DataLen
 Command payload length.
 
uint8_t * pData
 Command payload.
 
uint16_t GPPAddress
 Address of the GPP that generates the Notification.
 
uint8_t GPPLink
 Link quality of between the GPD and GPP.
 
uint32_t MIC
 MIC value for security failed frames.
 

The documentation for this struct was generated from the following file: