TI-15.4 Stack API
Data Fields
_apimac_mlmesynclossind Struct Reference

#include <api_mac.h>

Collaboration diagram for _apimac_mlmesynclossind:
Collaboration graph
[legend]

Data Fields

ApiMac_status_t reason
 
uint16_t panId
 
uint8_t logicalChannel
 
uint8_t channelPage
 
uint8_t phyID
 
ApiMac_sec_t sec
 

Detailed Description

MAC_MLME_SYNC_LOSS_IND type

Field Documentation

§ reason

ApiMac_status_t _apimac_mlmesynclossind::reason

Reason that the synchronization was lost

§ panId

uint16_t _apimac_mlmesynclossind::panId

The PAN ID of the realignment

§ logicalChannel

uint8_t _apimac_mlmesynclossind::logicalChannel

The logical channel of the realignment

§ channelPage

uint8_t _apimac_mlmesynclossind::channelPage

The channel page of the realignment

§ phyID

uint8_t _apimac_mlmesynclossind::phyID

PHY ID corresponding to the PHY descriptor of the realignment

§ sec

ApiMac_sec_t _apimac_mlmesynclossind::sec

The security parameters for this message


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale