![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
SNP GAP Layer API.
This file contains the interface to the SNP GAP Layer
Go to the source code of this file.
Functions | |
uint8_t | SNP_getGapParam (snpGetGapParamReq_t *cmdStruct) |
SNP Get GAP Parameter. More... | |
uint8_t | SNP_sendSecurityRequest (void) |
SNP Send Security Request. More... | |
uint8_t | SNP_setAdvData (snpSetAdvDataReq_t *cmdData, uint8_t len) |
SNP Set Advertisement Data. More... | |
uint8_t | SNP_setAuthenticationData (snpSetAuthDataReq_t *pReq) |
SNP Set Authentication Data. More... | |
uint8_t | SNP_setGapParam (snpSetGapParamReq_t *cmdStruct) |
SNP Set GAP Parameter. More... | |
uint8_t | SNP_setSecurityParams (snpSetSecParamReq_t *pReq) |
SNP Set Security Parameters. More... | |
uint8_t | SNP_setWhiteListFilterPolicy (snpSetWhiteListReq_t *pReq) |
SNP Set White List Filter Policy. More... | |
uint8_t | SNP_startAdv (snpStartAdvReq_t *cmdStartAdv) |
SNP Start Advertisement. More... | |
uint8_t | SNP_stopAdv (void) |
SNP Stop Advertisement. More... | |
uint8_t | SNP_terminateConn (snpTermConnReq_t *cmdStruct) |
SNP Terminate Connection. More... | |
uint8_t | SNP_updateConnParam (snpUpdateConnParamReq_t *cmdData) |
SNP Update Connection Parameters. More... | |