61 #ifndef SIMPLEPROCESSOR_GAP_H 62 #define SIMPLEPROCESSOR_GAP_H Parameter Structure for SNP_updateConnParam.
Definition: snp.h:744
uint8_t SNP_setSecurityParams(snpSetSecParamReq_t *pReq)
SNP Set Security Parameters.
Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ.
Definition: snp.h:851
uint8_t SNP_stopAdv(void)
SNP Stop Advertisement.
uint8_t SNP_startAdv(snpStartAdvReq_t *cmdStartAdv)
SNP Start Advertisement.
uint8_t SNP_setAuthenticationData(snpSetAuthDataReq_t *pReq)
SNP Set Authentication Data.
uint8_t SNP_updateConnParam(snpUpdateConnParamReq_t *cmdData)
SNP Update Connection Parameters.
uint8_t SNP_setGapParam(snpSetGapParamReq_t *cmdStruct)
SNP Set GAP Parameter.
Parameter Structure for SNP_setWhiteListFilterPolicy / SNP_SET_WHITE_LIST_POLICY_REQ.
Definition: snp.h:1355
uint8_t SNP_terminateConn(snpTermConnReq_t *cmdStruct)
SNP Terminate Connection.
uint8_t SNP_sendSecurityRequest(void)
SNP Send Security Request.
uint8_t SNP_getGapParam(snpGetGapParamReq_t *cmdStruct)
SNP Get GAP Parameter.
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.
Definition: snp.h:818
Connection Termination Request Structure.
Definition: snp.h:731
Parameter Structure for SNP_startAdv.
Definition: snp.h:691
Parameter Structure for SNP_setAdvData.
Definition: snp.h:716
uint8_t SNP_setAdvData(snpSetAdvDataReq_t *cmdData, uint8_t len)
SNP Set Advertisement Data.
uint8_t SNP_setWhiteListFilterPolicy(snpSetWhiteListReq_t *pReq)
SNP Set White List Filter Policy.